Difference between packaging

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Difference between packaging

1,294 次查看
johynpapin
Contributor I

Hello.
This question may sound silly, but I would like to have more information about the i.MX7 packages difference.
What is the advantage of the 19 * 19mm version given that the 12 * 12 is cheaper?

Best regards, Johyn Papin.

标签 (1)
0 项奖励
回复
1 回复

1,246 次查看
b36401
NXP Employee
NXP Employee

Please note that these package differs a bit with pin configuration.
For example 12x12 one has no pins related to ADC2.
Please refer pitch ball map you can find in the Datasheet.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复