Difference between packaging

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Difference between packaging

1,303件の閲覧回数
johynpapin
Contributor I

Hello.
This question may sound silly, but I would like to have more information about the i.MX7 packages difference.
What is the advantage of the 19 * 19mm version given that the 12 * 12 is cheaper?

Best regards, Johyn Papin.

ラベル(1)
0 件の賞賛
返信
1 返信

1,255件の閲覧回数
b36401
NXP Employee
NXP Employee

Please note that these package differs a bit with pin configuration.
For example 12x12 one has no pins related to ADC2.
Please refer pitch ball map you can find in the Datasheet.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信