Difference between Mfgtool with rootfs and without rootfs

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Difference between Mfgtool with rootfs and without rootfs

2,315件の閲覧回数
adityanagal
Contributor III

HI ,

I want to flash my target board having SDcard  using MFGtool . I downloaded the MFgtool  L4.1.15_2.0.0-ga_mfg-tools  from NXP site. This packages  has two folders  mfgtools-with-rootfs  and mfgtools-without-rootfs . My questions are as follows :-

1.  Both the folders having MFGtool.exe , so what's the difference is these two.

2.  Can I use this package for flashing the IMX6 based target board .

Please suggest.

Regards,

Aditya Nagal

0 件の賞賛
返信
1 返信

1,754件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

Hi Aditya,

What board are you using?

Please note that MFGtool was developed to be used with our evaluation boards. If you want to use MFGtool with a custom board you need to build an image that Yocto provides with all the settings to be used with MFGtool and edit it with you ddr settings.

Please find below some discussions and documents about this:

MFGTool for custom i.MX6SL board 

Custom board MFG tool support 

i.MX6 DDR Stress Test Tool V1.0.3 

i.MX6DQSDL DDR3 Script Aid 


Best regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信