Device mounting problem as mass storage on Windows

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Device mounting problem as mass storage on Windows

Jump to solution
1,692 Views
avijitnsec
Contributor III

I have downloaded Yocto image in SD Card and created 2 more partitions on the SD card. I am using iMX8mm platform.

I am mounting both the partitions using mass storage module - modprobe g_mass_storage file=/dev/mmcblk1p3,/dev/mmcblk1p5

I was hoping to get both the partitions mounted as mass storage device when connected through USB.

On Windows machine, only one partition being mounted. On Ubuntu machine, both the partitions being mounted.

I am able to mount individual partitions using the following commands

mount /dev/mmcblk1p3 /mnt

mount /dev/mmcblk1p5 /mnt

They both are FAT32. If I insert the SD Card directly to Windows machine, they mount just fine. And if I mount them one at a time, they both are mounting properly.

Any idea what is going wrong with Windows machine ? How to consistently mount both the partition on all the platforms ?

0 Kudos
Reply
1 Solution
1,674 Views
b36401
NXP Employee
NXP Employee

Please note that Windows does not support more than one partition on USB flash drive (which is emulated by i.MX board).

View solution in original post

0 Kudos
Reply
1 Reply
1,675 Views
b36401
NXP Employee
NXP Employee

Please note that Windows does not support more than one partition on USB flash drive (which is emulated by i.MX board).

0 Kudos
Reply