Development time under yocto

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Development time under yocto

1,628件の閲覧回数
christophe
Contributor V

Hi all,

We're using yocto to develop for a few weeks and find it very cumbersome. No trouble with the patch process and the general scheme of development. No, the problem is working with yocto is blatantly time-consuming... for nothing, spending time to compile and compile again full modules whereas only one file has been touched .

Yocto doesn't see a modified file and thus, the whole module has to be recompiled at each time. As it is often the kernel, it's very long. And seemingly, it's not possible to change this fact.

I'm very upset with this behaviour, and i wonder how to bypass it, if possible.

Some people suggest to develop elsewhere than in yocto. So, is there an obvious solution, that would be linked with yocto ? Or do we need to roughly copy sources into another development environment like Ltib ? Buildroot ? Other ?

Rgds,

Christophe

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

1,484件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Christophe

it may be more suitable to post it to meta-fsl-arm mailing list,

so that yocto developers could try to assist you.
https://lists.yoctoproject.org/listinfo/meta-freescale
Ltib is not more supported by nxp, also buildroot. For buildroot one can look on

Buildroot for the i.MX6 sabre sd platform in a few commands 

Buildroot for i.MX5 and i.MX6 - Boundary Devices 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,484件の閲覧回数
christophe
Contributor V

Thanks Igor.

0 件の賞賛
返信