Development platform running Android Wear OS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Development platform running Android Wear OS

ソリューションへジャンプ
2,269件の閲覧回数
lyfsci
Contributor III

Hi Experts,

Is there any development platform in IMX or Freescale chips supporting the Android Wear OS ?

Regards,

Lyf

ラベル(1)
0 件の賞賛
返信
1 解決策
2,067件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

So far there is no plan in our roadmap to support android wear so far. Good thing here is that once it's in our roadmap, it won't be much of a work to do it since it requires full android support, which we do.


Have a great day,
Sergio Solis

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,068件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

So far there is no plan in our roadmap to support android wear so far. Good thing here is that once it's in our roadmap, it won't be much of a work to do it since it requires full android support, which we do.


Have a great day,
Sergio Solis

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信