Development platform running Android Wear OS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Development platform running Android Wear OS

Jump to solution
2,324 Views
lyfsci
Contributor III

Hi Experts,

Is there any development platform in IMX or Freescale chips supporting the Android Wear OS ?

Regards,

Lyf

Labels (1)
0 Kudos
Reply
1 Solution
2,122 Views
SergioSolis
NXP Employee
NXP Employee

So far there is no plan in our roadmap to support android wear so far. Good thing here is that once it's in our roadmap, it won't be much of a work to do it since it requires full android support, which we do.


Have a great day,
Sergio Solis

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
2,123 Views
SergioSolis
NXP Employee
NXP Employee

So far there is no plan in our roadmap to support android wear so far. Good thing here is that once it's in our roadmap, it won't be much of a work to do it since it requires full android support, which we do.


Have a great day,
Sergio Solis

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply