Design guide for i.MX 7ULP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Design guide for i.MX 7ULP

1,348 Views
stanley_wissmar
Contributor I

How/where is the design guide (and datasheet) available for the i.MX 7ULP processor?

Labels (1)
0 Kudos
Reply
1 Reply

1,255 Views
art
NXP Employee
NXP Employee

Since the i.MX7ULP processor is still in pre-production stage, no detailed documentation is publicly available for it yet. The documentation will become avaialable at the moment of the processor's official launch that is scheduled to the end of June 2019.


Have a great day,
Artur

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply