Design guide for i.MX 7ULP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Design guide for i.MX 7ULP

1,345件の閲覧回数
stanley_wissmar
Contributor I

How/where is the design guide (and datasheet) available for the i.MX 7ULP processor?

ラベル(1)
0 件の賞賛
返信
1 返信

1,252件の閲覧回数
art
NXP Employee
NXP Employee

Since the i.MX7ULP processor is still in pre-production stage, no detailed documentation is publicly available for it yet. The documentation will become avaialable at the moment of the processor's official launch that is scheduled to the end of June 2019.


Have a great day,
Artur

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信