Default setting of MIPI-CSI2 virtual channel 0 (part2)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Default setting of MIPI-CSI2 virtual channel 0 (part2)

ソリューションへジャンプ
1,637件の閲覧回数
torus1000
Contributor V

Please see previous thread already closed.
https://community.freescale.com/message/425008

  (Q) Which one is correct a) VC0 merely connect to IPU1_CSI0 or
      b) VC0 is one of choice for IPU1_CSI1?

  (A) a) is correct.
--------------------------------------------------------------

Dear Yuri and members,

I made a big mistake because my customer used not ltib but yocto.

I agree with the answer should be same but...

Could you explain one more time with yocto source?

Sorry for waste your time. I think dtsi include same information.

Here: fsl-release-bsp/build/tmp/work/imx6qsabresd-poky-*/linux-imx/3.10.17-r0/git/arch/arm/boot/dts/imx6q*sd.dtsi


Thanks.

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
1,285件の閲覧回数
Yuri
NXP Employee
NXP Employee

1.

You are right, VC0 relates to IPU1_CSI0 (IPU1/2), according to the .dtsi file.

2.

For i.MX6 DQ only IPU1_CSI0 can be associated with VC0 ; please take a look

at IMOUX GPR (bit 19) description.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,286件の閲覧回数
Yuri
NXP Employee
NXP Employee

1.

You are right, VC0 relates to IPU1_CSI0 (IPU1/2), according to the .dtsi file.

2.

For i.MX6 DQ only IPU1_CSI0 can be associated with VC0 ; please take a look

at IMOUX GPR (bit 19) description.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信