Default setting of MIPI-CSI2 virtual channel 0 (part2)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Default setting of MIPI-CSI2 virtual channel 0 (part2)

跳至解决方案
1,638 次查看
torus1000
Contributor V

Please see previous thread already closed.
https://community.freescale.com/message/425008

  (Q) Which one is correct a) VC0 merely connect to IPU1_CSI0 or
      b) VC0 is one of choice for IPU1_CSI1?

  (A) a) is correct.
--------------------------------------------------------------

Dear Yuri and members,

I made a big mistake because my customer used not ltib but yocto.

I agree with the answer should be same but...

Could you explain one more time with yocto source?

Sorry for waste your time. I think dtsi include same information.

Here: fsl-release-bsp/build/tmp/work/imx6qsabresd-poky-*/linux-imx/3.10.17-r0/git/arch/arm/boot/dts/imx6q*sd.dtsi


Thanks.

标签 (1)
标记 (3)
0 项奖励
回复
1 解答
1,286 次查看
Yuri
NXP Employee
NXP Employee

1.

You are right, VC0 relates to IPU1_CSI0 (IPU1/2), according to the .dtsi file.

2.

For i.MX6 DQ only IPU1_CSI0 can be associated with VC0 ; please take a look

at IMOUX GPR (bit 19) description.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,287 次查看
Yuri
NXP Employee
NXP Employee

1.

You are right, VC0 relates to IPU1_CSI0 (IPU1/2), according to the .dtsi file.

2.

For i.MX6 DQ only IPU1_CSI0 can be associated with VC0 ; please take a look

at IMOUX GPR (bit 19) description.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复