Debugging U-boot on IMX6ULL using JTAG

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debugging U-boot on IMX6ULL using JTAG

11,300件の閲覧回数
Almaz
Contributor I

Hello.

Trying to debug U-boot on IMX6ULL using this manual.

So I am able to compile U-boot sources using Eclipse and get binary U-boot file.

Enabled debugging options in .config file:

 

CONFIG_CC_OPTIMIZE_FOR_SIZE=n
CONFIG_TOOLS_DEBUG=y

 

Here debugger configuration:

Screenshot from 2021-09-08 23-29-07.pngScreenshot from 2021-09-08 23-29-07.png

Screenshot from 2021-09-08 23-29-27.pngScreenshot from 2021-09-08 23-29-27.png

Screenshot from 2021-09-08 23-29-46.pngScreenshot from 2021-09-08 23-29-46.png

 Get following logs on starting debugger server:

 

SEGGER J-Link GDB Server V7.54a Command Line Version

JLinkARM.dll V7.54a (DLL compiled Sep  7 2021 14:25:38)

Command line: -if jtag -device MCIMX6Y2 -endian little -speed auto -port 2331 -swoport 2332 -telnetport 2333 -noir -localhostonly 0 -scriptfile ddr_init.jlinkscript
-----GDB Server start settings-----
GDBInit file:                  none
GDB Server Listening port:     2331
SWO raw output listening port: 2332
Terminal I/O port:             2333
Accept remote connection:      yes
Generate logfile:              off
Verify download:               off
Init regs on start:            off
Silent mode:                   off
Single run mode:               off
Target connection timeout:     0 ms
------J-Link related settings------
J-Link Host interface:         USB
J-Link script:                 ddr_init.jlinkscript
J-Link settings file:          none
------Target related settings------
Target device:                 MCIMX6Y2
Target interface:              JTAG
Target interface speed:        auto
Target endian:                 little

Connecting to J-Link...
J-Link is connected.
Firmware: J-Link ARM V8 compiled Nov 28 2014 13:44:46
Hardware: V8.00
Feature(s): RDI,FlashDL,FlashBP,JFlash,GDB
Checking target voltage...
Target voltage: 3.26 V
Listening on TCP/IP port 2331
Connecting to target...

J-Link found 3 JTAG devices, Total IRLen = 13
JTAG ID: 0x5BA00477 (Cortex-A7)
Connected to target
Waiting for GDB connection...Connected to 127.0.0.1
Reading all registers
Read 4 bytes @ address 0x87890988 (Data = 0x00000000)
Read 4 bytes @ address 0x8785F178 (Data = 0xEAFFFFFE)
Read 4 bytes @ address 0x8785F174 (Data = 0xEBFED7AE)
Read 4 bytes @ address 0x8785F178 (Data = 0xEAFFFFFE)
Read 4 bytes @ address 0x8785F174 (Data = 0xEBFED7AE)
Read 2 bytes @ address 0x8785F178 (Data = 0xFFFE)
Read 2 bytes @ address 0x8785F176 (Data = 0xEBFE)
Read 2 bytes @ address 0x8785F174 (Data = 0xD7AE)
Read 2 bytes @ address 0x8785F178 (Data = 0xFFFE)
Read 2 bytes @ address 0x8785F176 (Data = 0xEBFE)
Read 2 bytes @ address 0x8785F174 (Data = 0xD7AE)
Read 4 bytes @ address 0x8785F178 (Data = 0xEAFFFFFE)
Read 4 bytes @ address 0x8785F174 (Data = 0xEBFED7AE)
Read 4 bytes @ address 0x8785F178 (Data = 0xEAFFFFFE)
Read 4 bytes @ address 0x8785F174 (Data = 0xEBFED7AE)
Read 4 bytes @ address 0x8785F178 (Data = 0xEAFFFFFE)
Read 4 bytes @ address 0x8785F178 (Data = 0xEAFFFFFE)
Read 4 bytes @ address 0x8785F178 (Data = 0xEAFFFFFE)
Received monitor command: speed 1000
Target interface speed set to 1000 kHz
Received monitor command: clrbp
Received monitor command: reset
Resetting target
Received monitor command: halt
Halting target CPU...
...Target halted (PC = 0x8785F178)
Received monitor command: regs
PC = 8785F178, CPSR = 600001D3 (SVC mode, ARM FIQ dis. IRQ dis.)
R0 = 8785F180, R1 = 8786F6B8, R2 = 00000000, R3 = 0091F78D
R4 = 00000005, R5 = 87800320, R6 = 00000001, R7 = 8FF8D5BA
USR: R8 =8FF9CC8C, R9 =0091FA00, R10=8FF8D5BA, R11 =00000001, R12 =00000031
     R13=80DB8C6B, R14=9E4F4394
FIQ: R8 =B6472704, R9 =846B1BF6, R10=DD3BACFE, R11 =EFF1EB7F, R12 =6E6C9283
     R13=DC9247E9, R14=1F5A8FEF, SPSR=5A000312
SVC: R13=0091F9F0, R14=8785F178, SPSR=000001D3
ABT: R13=CDF44348, R14=6CA56019, SPSR=10038120
IRQ: R13=E966343D, R14=2AC8E2B6, SPSR=38026A20
UND: R13=7FC7CC2D, R14=11E13C9D, SPSR=20066601
Reading all registers
Received monitor command: speed auto
Select auto target interface speed (1000 kHz)
Received monitor command: flash breakpoints 1
Flash breakpoints enabled
Received monitor command: semihosting enable
Semi-hosting enabled (SVC Addr = 0x08)
Received monitor command: semihosting IOClient 2
Semihosting I/O set to GDB Client
Read 4 bytes @ address 0x87890988 (Data = 0x00000000)
Downloading 16272 bytes @ address 0x87800000
Downloading 16304 bytes @ address 0x87803F90
Downloading 16304 bytes @ address 0x87807F40
Downloading 16272 bytes @ address 0x8780BEF0
Downloading 16304 bytes @ address 0x8780FE80
Downloading 16272 bytes @ address 0x87813E30
Downloading 16288 bytes @ address 0x87817DC0
Downloading 16240 bytes @ address 0x8781BD60
Downloading 16272 bytes @ address 0x8781FCD0
Downloading 16272 bytes @ address 0x87823C60
Downloading 16256 bytes @ address 0x87827BF0
Downloading 16288 bytes @ address 0x8782BB70
Downloading 16272 bytes @ address 0x8782FB10
Downloading 16272 bytes @ address 0x87833AA0
Downloading 16256 bytes @ address 0x87837A30
Downloading 16256 bytes @ address 0x8783B9B0
Downloading 16256 bytes @ address 0x8783F930
Downloading 16304 bytes @ address 0x878438B0
Downloading 16288 bytes @ address 0x87847860
Downloading 16272 bytes @ address 0x8784B800
Downloading 16256 bytes @ address 0x8784F790
Downloading 16288 bytes @ address 0x87853710
Downloading 16160 bytes @ address 0x878576B0
Downloading 16192 bytes @ address 0x8785B5D0
Downloading 16272 bytes @ address 0x8785F510
Downloading 16272 bytes @ address 0x878634A0
Downloading 40 bytes @ address 0x87867430
Downloading 16120 bytes @ address 0x87867458
Downloading 16224 bytes @ address 0x8786B350
Downloading 16192 bytes @ address 0x8786F2B0
Downloading 16336 bytes @ address 0x878731F0
Downloading 16336 bytes @ address 0x878771C0
Downloading 1294 bytes @ address 0x8787B190
Downloading 24 bytes @ address 0x8787B6A0
Downloading 16328 bytes @ address 0x8787B6B8
Downloading 11484 bytes @ address 0x8787F680
Downloading 12 bytes @ address 0x8788235C
Downloading 4616 bytes @ address 0x87882368
Downloading 256 bytes @ address 0x87883570
Downloading 144 bytes @ address 0x87883670
Downloading 16256 bytes @ address 0x87883700
Downloading 16304 bytes @ address 0x87887680
Downloading 16304 bytes @ address 0x8788B630
Downloading 4928 bytes @ address 0x8788F5E0
Downloading 48 bytes @ address 0x87890920
Downloading 1 bytes @ address 0x87890950
Downloading 144 bytes @ address 0x87890954
Downloading 24 bytes @ address 0x878909E4
Writing register (PC = 0x87800000)
Read 4 bytes @ address 0x87800000 (Data = 0xEA0000B8)
Read 4 bytes @ address 0x877FFFFC (Data = 0x00000000)
Read 4 bytes @ address 0x87800000 (Data = 0xEA0000B8)
Read 4 bytes @ address 0x877FFFFC (Data = 0x00000000)
Read 2 bytes @ address 0x87800000 (Data = 0x00B8)
Read 2 bytes @ address 0x877FFFFE (Data = 0x0000)
Read 2 bytes @ address 0x877FFFFC (Data = 0x0000)
Read 2 bytes @ address 0x87800000 (Data = 0x00B8)
Read 2 bytes @ address 0x877FFFFE (Data = 0x0000)
Read 2 bytes @ address 0x877FFFFC (Data = 0x0000)
Read 4 bytes @ address 0x87800000 (Data = 0xEA0000B8)
Read 4 bytes @ address 0x877FFFFC (Data = 0x00000000)
Read 4 bytes @ address 0x87800000 (Data = 0xEA0000B8)
Read 4 bytes @ address 0x877FFFFC (Data = 0x00000000)
Read 4 bytes @ address 0x87800000 (Data = 0xEA0000B8)
Read 4 bytes @ address 0x87800000 (Data = 0xEA0000B8)
Read 4 bytes @ address 0x87800000 (Data = 0xEA0000B8)
Read 4 bytes @ address 0x87800000 (Data = 0xEA0000B8)
Read 4 bytes @ address 0x8781503C (Data = 0xE52DE004)
Reading 64 bytes @ address 0x87817CC0
Read 4 bytes @ address 0x87817CD8 (Data = 0x8786811C)
Read 4 bytes @ address 0x87817CC8 (Data = 0xE59F0008)
Reading 64 bytes @ address 0x87818080
Read 4 bytes @ address 0x8781809C (Data = 0xE59F0004)
Reading 64 bytes @ address 0x87817E80
Read 4 bytes @ address 0x87817EA4 (Data = 0xEBFFF464)
Read 4 bytes @ address 0x87817EA0 (Data = 0xE92D4010)
Received monitor command: regs
PC = 87800000, CPSR = 600001D3 (SVC mode, ARM FIQ dis. IRQ dis.)
R0 = 8785F180, R1 = 8786F6B8, R2 = 00000000, R3 = 0091F78D
R4 = 00000005, R5 = 87800320, R6 = 00000001, R7 = 8FF8D5BA
USR: R8 =8FF9CC8C, R9 =0091FA00, R10=8FF8D5BA, R11 =00000001, R12 =00000031
     R13=80DB8C6B, R14=9E4F4394
FIQ: R8 =B6472704, R9 =846B1BF6, R10=DD3BACFE, R11 =EFF1EB7F, R12 =6E6C9283
     R13=DC9247E9, R14=1F5A8FEF, SPSR=5A000312
SVC: R13=0091F9F0, R14=8785F178, SPSR=000001D3
ABT: R13=CDF44348, R14=6CA56019, SPSR=10038120
IRQ: R13=E966343D, R14=2AC8E2B6, SPSR=38026A20
UND: R13=7FC7CC2D, R14=11E13C9D, SPSR=20066601
Reading all registers
Read 4 bytes @ address 0x87800000 (Data = 0xEA0000B8)
Read 4 bytes @ address 0x877FFFFC (Data = 0x00000000)
Read 4 bytes @ address 0x87800000 (Data = 0xEA0000B8)
Read 4 bytes @ address 0x877FFFFC (Data = 0x00000000)
Read 2 bytes @ address 0x87800000 (Data = 0x00B8)
Read 2 bytes @ address 0x877FFFFE (Data = 0x0000)
Read 2 bytes @ address 0x877FFFFC (Data = 0x0000)
Read 2 bytes @ address 0x87800000 (Data = 0x00B8)
Read 2 bytes @ address 0x877FFFFE (Data = 0x0000)
Read 2 bytes @ address 0x877FFFFC (Data = 0x0000)
Read 4 bytes @ address 0x87800000 (Data = 0xEA0000B8)
Read 4 bytes @ address 0x877FFFFC (Data = 0x00000000)
Read 4 bytes @ address 0x87800000 (Data = 0xEA0000B8)
Read 4 bytes @ address 0x877FFFFC (Data = 0x00000000)
Read 4 bytes @ address 0x87800000 (Data = 0xEA0000B8)
Read 4 bytes @ address 0x87800000 (Data = 0xEA0000B8)
Read 4 bytes @ address 0x87800000 (Data = 0xEA0000B8)
Read 4 bytes @ address 0x87800000 (Data = 0xEA0000B8)

 

Everything looks fine but unfortunately get following error message at debugging window:

Screenshot from 2021-09-08 23-27-17.pngScreenshot from 2021-09-08 23-27-17.png

Another one thing confusing me is that u-boot console still accessible to enter commands and no reboot messages in console during startng debugging session.

Any hints what did I miss?

0 件の賞賛
返信
5 返答(返信)

11,291件の閲覧回数
igorpadykov
NXP Employee
NXP Employee
0 件の賞賛
返信

11,283件の閲覧回数
Almaz
Contributor I

Thank you very much for links, Igor!

Checked them carefully. But still can't debug properly.

As there are troubles with Eclipse I decided to try from scratch, e.g. tried to debug from command line.

Here what I did.

Started JLinkGDBServer:

$ JLinkGDBServer -device MCIMX6Y2 -if JTAG -speed 1000

with following logs:

SEGGER J-Link GDB Server V7.54a Command Line Version

JLinkARM.dll V7.54a (DLL compiled Sep  7 2021 14:25:38)

Command line: -device MCIMX6Y2 -if JTAG -speed 1000
-----GDB Server start settings-----
GDBInit file:                  none
GDB Server Listening port:     2331
SWO raw output listening port: 2332
Terminal I/O port:             2333
Accept remote connection:      yes
Generate logfile:              off
Verify download:               off
Init regs on start:            off
Silent mode:                   off
Single run mode:               off
Target connection timeout:     0 ms
------J-Link related settings------
J-Link Host interface:         USB
J-Link script:                 none
J-Link settings file:          none
------Target related settings------
Target device:                 MCIMX6Y2
Target interface:              JTAG
Target interface speed:        1000kHz
Target endian:                 little

Connecting to J-Link...
J-Link is connected.
Firmware: J-Link ARM V8 compiled Nov 28 2014 13:44:46
Hardware: V8.00
Feature(s): RDI,FlashDL,FlashBP,JFlash,GDB
Checking target voltage...
Target voltage: 3.26 V
Listening on TCP/IP port 2331
Connecting to target...

J-Link found 3 JTAG devices, Total IRLen = 13
JTAG ID: 0x5BA00477 (Cortex-A7)
Connected to target
Waiting for GDB connection...

then I created gdb init script based on lauterbach's dcd files and script provided there:

# Initializing target
target remote localhost:2331
monitor reset
monitor halt
monitor sleep 200

# Disable Watchdog
monitor memU32 0x020bc000=0x30
                                                     
# Enable all clocks
monitor memU32 0x020c4068=0xffffffff
monitor memU32 0x020c406c=0xffffffff
monitor memU32 0x020c4070=0xffffffff
monitor memU32 0x020c4074=0xffffffff
monitor memU32 0x020c4078=0xffffffff
monitor memU32 0x020c407c=0xffffffff
monitor memU32 0x020c4080=0xffffffff

monitor memU32 0x020E04B4=0x000C0000
monitor memU32 0x020E04AC=0x00000000
monitor memU32 0x020E027C=0x00000030
monitor memU32 0x020E0250=0x00000030
monitor memU32 0x020E024C=0x00000030
monitor memU32 0x020E0490=0x00000030
monitor memU32 0x020E0288=0x000C0030
monitor memU32 0x020E0270=0x00000000
monitor memU32 0x020E0260=0x00000030
monitor memU32 0x020E0264=0x00000030
monitor memU32 0x020E04A0=0x00000030
monitor memU32 0x020E0494=0x00020000
monitor memU32 0x020E0280=0x00000030
monitor memU32 0x020E0284=0x00000030
monitor memU32 0x020E04B0=0x00020000
monitor memU32 0x020E0498=0x00000030
monitor memU32 0x020E04A4=0x00000030
monitor memU32 0x020E0244=0x00000030
monitor memU32 0x020E0248=0x00000030
monitor memU32 0x021B001C=0x00008000
monitor memU32 0x021B0800=0xA1390003
monitor memU32 0x021B080C=0x00000004
monitor memU32 0x021B083C=0x41640158
monitor memU32 0x021B0848=0x40403237
monitor memU32 0x021B0850=0x40403C33
monitor memU32 0x021B081C=0x33333333
monitor memU32 0x021B0820=0x33333333
monitor memU32 0x021B082C=0xf3333333
monitor memU32 0x021B0830=0xf3333333
monitor memU32 0x021B08C0=0x00944009
monitor memU32 0x021B08b8=0x00000800
monitor memU32 0x021B0004=0x0002002D
monitor memU32 0x021B0008=0x1B333030
monitor memU32 0x021B000C=0x676B52F3
monitor memU32 0x021B0010=0xB66D0B63
monitor memU32 0x021B0014=0x01FF00DB
monitor memU32 0x021B0018=0x00201740
monitor memU32 0x021B001C=0x00008000
monitor memU32 0x021B002C=0x000026D2
monitor memU32 0x021B0030=0x006B1023
monitor memU32 0x021B0040=0x0000004F
monitor memU32 0x021B0000=0x84180000
monitor memU32 0x021B0890=0x00400000
monitor memU32 0x021B001C=0x02008032
monitor memU32 0x021B001C=0x00008033
monitor memU32 0x021B001C=0x00048031
monitor memU32 0x021B001C=0x15208030
monitor memU32 0x021B001C=0x04008040
monitor memU32 0x021B0020=0x00000800
monitor memU32 0x021B0818=0x00000227
monitor memU32 0x021B0004=0x0002552D
monitor memU32 0x021B0404=0x00011006
monitor memU32 0x021B001C=0x00000000

monitor reg cpsr = 0xD3
monitor reg sp = 0x0093FF20
monitor reg pc = 0x87800000

here is command I start gdb:

$ gdb-multiarch u-boot --nx -ix lauterbach

and it outputs:

0x8ff62d00 in ?? ()
Resetting target
Sleep 200ms
Writing 0x00000030 @ address 0x020BC000
Writing 0xFFFFFFFF @ address 0x020C4068
Writing 0xFFFFFFFF @ address 0x020C406C
Writing 0xFFFFFFFF @ address 0x020C4070
Writing 0xFFFFFFFF @ address 0x020C4074
Writing 0xFFFFFFFF @ address 0x020C4078
Writing 0xFFFFFFFF @ address 0x020C407C
Writing 0xFFFFFFFF @ address 0x020C4080
Writing 0x000C0000 @ address 0x020E04B4
Writing 0x00000000 @ address 0x020E04AC
Writing 0x00000030 @ address 0x020E027C
Writing 0x00000030 @ address 0x020E0250
Writing 0x00000030 @ address 0x020E024C
Writing 0x00000030 @ address 0x020E0490
Writing 0x000C0030 @ address 0x020E0288
Writing 0x00000000 @ address 0x020E0270
Writing 0x00000030 @ address 0x020E0260
Writing 0x00000030 @ address 0x020E0264
Writing 0x00000030 @ address 0x020E04A0
Writing 0x00020000 @ address 0x020E0494
Writing 0x00000030 @ address 0x020E0280
Writing 0x00000030 @ address 0x020E0284
Writing 0x00020000 @ address 0x020E04B0
Writing 0x00000030 @ address 0x020E0498
Writing 0x00000030 @ address 0x020E04A4
Writing 0x00000030 @ address 0x020E0244
Writing 0x00000030 @ address 0x020E0248
Writing 0x00008000 @ address 0x021B001C
Writing 0xA1390003 @ address 0x021B0800
Writing 0x00000004 @ address 0x021B080C
Writing 0x41640158 @ address 0x021B083C
Writing 0x40403237 @ address 0x021B0848
Writing 0x40403C33 @ address 0x021B0850
Writing 0x33333333 @ address 0x021B081C
Writing 0x33333333 @ address 0x021B0820
Writing 0xF3333333 @ address 0x021B082C
Writing 0xF3333333 @ address 0x021B0830
Writing 0x00944009 @ address 0x021B08C0
Writing 0x00000800 @ address 0x021B08B8
Writing 0x0002002D @ address 0x021B0004
Writing 0x1B333030 @ address 0x021B0008
Writing 0x676B52F3 @ address 0x021B000C
Writing 0xB66D0B63 @ address 0x021B0010
Writing 0x01FF00DB @ address 0x021B0014
Writing 0x00201740 @ address 0x021B0018
Writing 0x00008000 @ address 0x021B001C
Writing 0x000026D2 @ address 0x021B002C
Writing 0x006B1023 @ address 0x021B0030
Writing 0x0000004F @ address 0x021B0040
Writing 0x84180000 @ address 0x021B0000
Writing 0x00400000 @ address 0x021B0890
Writing 0x02008032 @ address 0x021B001C
Writing 0x00008033 @ address 0x021B001C
Writing 0x00048031 @ address 0x021B001C
Writing 0x15208030 @ address 0x021B001C
Writing 0x04008040 @ address 0x021B001C
Writing 0x00000800 @ address 0x021B0020
Writing 0x00000227 @ address 0x021B0818
Writing 0x0002552D @ address 0x021B0004
Writing 0x00011006 @ address 0x021B0404
Writing 0x00000000 @ address 0x021B001C
Writing register (F0 = 0x000000D3)
Writing register (SP = 0x0093FF20)
Writing register (PC = 0x87800000)
Reading symbols from u-boot...

then I:

(gdb) load
Loading section .text, size 0x67458 lma 0x87800000
Loading section .rodata, size 0x14246 lma 0x87867458
Loading section .hash, size 0x18 lma 0x8787b6a0
Loading section .data, size 0x6ca4 lma 0x8787b6b8
Loading section .got.plt, size 0xc lma 0x8788235c
Loading section .u_boot_list, size 0x1208 lma 0x87882368
Loading section .efi_runtime, size 0x100 lma 0x87883570
Loading section .efi_runtime_rel, size 0x90 lma 0x87883670
Loading section .rel.dyn, size 0xd220 lma 0x87883700
Loading section .dynsym, size 0x30 lma 0x87890920
Loading section .dynstr, size 0x1 lma 0x87890950
Loading section .dynamic, size 0x90 lma 0x87890954
Loading section .gnu.hash, size 0x18 lma 0x878909e4
Start address 0x87800000, load size 592375
Transfer rate: 718 KB/sec, 12341 bytes/write.

and:

(gdb) s
Cannot access memory at address 0x87800000

while gdb server:

WARNING: Failed to read memory @ address 0x87800000
WARNING: Failed to read memory @ address 0x877FFFFC
WARNING: Failed to read memory @ address 0x87800000
WARNING: Failed to read memory @ address 0x877FFFFC
WARNING: Failed to read memory @ address 0x87800000
WARNING: Failed to read memory @ address 0x877FFFFE
WARNING: Failed to read memory @ address 0x877FFFFC
WARNING: Failed to read memory @ address 0x87800000
WARNING: Failed to read memory @ address 0x877FFFFE
WARNING: Failed to read memory @ address 0x877FFFFC
WARNING: Failed to read memory @ address 0x87800000
WARNING: Failed to read memory @ address 0x877FFFFC
WARNING: Failed to read memory @ address 0x87800000
WARNING: Failed to read memory @ address 0x877FFFFC
WARNING: Failed to read memory @ address 0x87800000
WARNING: Failed to read memory @ address 0x87800000
WARNING: Failed to read memory @ address 0x87800000
WARNING: Failed to read memory @ address 0x87800000

Unable to access DDR memory.

After that I rebooted device, restarted GDB server using same command an started gdb in following way:

$ gdb-multiarch u-boot --nx

and typed:

(gdb) target remote localhost:2331
Remote debugging using localhost:2331
0x8ff62d00 in ?? ()
(gdb) monitor reset
Resetting target
(gdb) monitor halt
(gdb) monitor sleep
Expected an decimal digit (0-9)
(gdb) monitor sleep 200
Sleep 200ms
(gdb) load
Loading section .text, size 0x67458 lma 0x87800000
Loading section .rodata, size 0x14246 lma 0x87867458
Loading section .hash, size 0x18 lma 0x8787b6a0
Loading section .data, size 0x6ca4 lma 0x8787b6b8
Loading section .got.plt, size 0xc lma 0x8788235c
Loading section .u_boot_list, size 0x1208 lma 0x87882368
Loading section .efi_runtime, size 0x100 lma 0x87883570
Loading section .efi_runtime_rel, size 0x90 lma 0x87883670
Loading section .rel.dyn, size 0xd220 lma 0x87883700
Loading section .dynsym, size 0x30 lma 0x87890920
Loading section .dynstr, size 0x1 lma 0x87890950
Loading section .dynamic, size 0x90 lma 0x87890954
Loading section .gnu.hash, size 0x18 lma 0x878909e4
Start address 0x87800000, load size 592375
Transfer rate: 69 KB/sec, 12341 bytes/write.

Then:

(gdb) s
reset () at arch/arm/cpu/armv7/start.S:40
40		b	save_boot_params
(gdb) s
save_boot_params () at arch/arm/cpu/armv7/start.S:116
116		b	save_boot_params_ret		@ back to my caller
(gdb) s
save_boot_params_ret () at arch/arm/cpu/armv7/start.S:56
56		mrs	r0, cpsr
(gdb) s
57		and	r1, r0, #0x1f		@ mask mode bits
(gdb) s
58		teq	r1, #0x1a		@ test for HYP mode

looks like I started to debug source code technically, but then:

Breakpoint 1 at 0x878020f4: file arch/arm/imx-common/cpu.c, line 184.
(gdb) c
Continuing.



s
c
^C
Program received signal SIGTRAP, Trace/breakpoint trap.
0x8785f178 in bootstage_error (id=BOOTSTAGE_ID_NEED_RESET) at include/bootstage.h:387
387		show_boot_progress(-id);

E.g. it stuck somewhere until I pressed CTRL-C.

Repeated GdbServer and gdb restarting and passed same steps and it exited at another source code line.

So I repeated everything again and went step by step:

Start address 0x87800000, load size 592375
Transfer rate: 69 KB/sec, 12341 bytes/write.
(gdb) s
reset () at arch/arm/cpu/armv7/start.S:40
40		b	save_boot_params
(gdb) s
save_boot_params () at arch/arm/cpu/armv7/start.S:116
116		b	save_boot_params_ret		@ back to my caller
(gdb) 
save_boot_params_ret () at arch/arm/cpu/armv7/start.S:56
56		mrs	r0, cpsr
(gdb) 
57		and	r1, r0, #0x1f		@ mask mode bits
(gdb) 
58		teq	r1, #0x1a		@ test for HYP mode
(gdb) 
59		bicne	r0, r0, #0x1f		@ clear all mode bits
(gdb) 
60		orrne	r0, r0, #0x13		@ set SVC mode
(gdb) s
61		orr	r0, r0, #0xc0		@ disable FIQ and IRQ
(gdb) s
62		msr	cpsr,r0
(gdb) s
71		mrc	p15, 0, r0, c1, c0, 0	@ Read CP15 SCTLR Register
(gdb) s
72		bic	r0, #CR_V		@ V = 0
(gdb) s
73		mcr	p15, 0, r0, c1, c0, 0	@ Write CP15 SCTLR Register
(gdb) s
76		ldr	r0, =_start
(gdb) s
77		mcr	p15, 0, r0, c12, c0, 0	@Set VBAR
(gdb) s
82		bl	cpu_init_cp15
(gdb) s
cpu_init_cp15 () at arch/arm/cpu/armv7/start.S:139
139		mov	r0, #0			@ set up for MCR
(gdb) s
140		mcr	p15, 0, r0, c8, c7, 0	@ invalidate TLBs
(gdb) s
141		mcr	p15, 0, r0, c7, c5, 0	@ invalidate icache
(gdb) s
142		mcr	p15, 0, r0, c7, c5, 6	@ invalidate BP array
(gdb) s
143		mcr     p15, 0, r0, c7, c10, 4	@ DSB
(gdb) s
144		mcr     p15, 0, r0, c7, c5, 4	@ ISB
(gdb) s
149		mrc	p15, 0, r0, c1, c0, 0
(gdb) s
150		bic	r0, r0, #0x00002000	@ clear bits 13 (--V-)
(gdb) s
151		bic	r0, r0, #0x00000007	@ clear bits 2:0 (-CAM)
(gdb) s
152		orr	r0, r0, #0x00000002	@ set bit 1 (--A-) Align
(gdb) s
153		orr	r0, r0, #0x00000800	@ set bit 11 (Z---) BTB
(gdb) s
157		orr	r0, r0, #0x00001000	@ set bit 12 (I) I-cache
(gdb) s
159		mcr	p15, 0, r0, c1, c0, 0
(gdb) s
190		mov	r5, lr			@ Store my Caller
(gdb) s
191		mrc	p15, 0, r1, c0, c0, 0	@ r1 has Read Main ID Register (MIDR)
(gdb) s
192		mov	r3, r1, lsr #20		@ get variant field
(gdb) s
193		and	r3, r3, #0xf		@ r3 has CPU variant
(gdb) s
194		and	r4, r1, #0xf		@ r4 has CPU revision
(gdb) s
195		mov	r2, r3, lsl #4		@ shift variant field for combined value
(gdb) s
196		orr	r2, r4, r2		@ r2 has combined CPU variant + revision
(gdb) s
298		mov	pc, r5			@ back to my caller
(gdb) s
save_boot_params_ret () at arch/arm/cpu/armv7/start.S:84
84		bl	cpu_init_crit
(gdb) s
cpu_init_crit () at arch/arm/cpu/armv7/start.S:318
318		b	lowlevel_init		@ go setup pll,mux,memory
(gdb) s
lowlevel_init () at arch/arm/cpu/armv7/lowlevel_init.S:32
32		ldr	sp, =CONFIG_SYS_INIT_SP_ADDR
(gdb) s
lowlevel_init () at arch/arm/cpu/armv7/lowlevel_init.S:34
34		bic	sp, sp, #7 /* 8-byte alignment for ABI compliance */
(gdb) s
45		sub	sp, sp, #GD_SIZE
(gdb) s
46		bic	sp, sp, #7
(gdb) s
47		mov	r9, sp
(gdb) s
53		push	{ip, lr}
(gdb) s
68		bl	s_init
(gdb) 
s_init () at arch/arm/cpu/armv7/mx6/soc.c:588
588		if (is_mx6sx() || is_mx6ul() || is_mx6ull())
(gdb) s
get_cpu_rev () at arch/arm/cpu/armv7/mx6/soc.c:69
69		u32 reg = readl(&anatop->digprog_sololite);
(gdb) s
70		u32 type = ((reg >> 16) & 0xff);
(gdb) 
73		if (type != MXC_CPU_MX6SL) {
(gdb) 
74			reg = readl(&anatop->digprog);
(gdb) 
76			cfg = readl(&scu->config) & 3;
(gdb) 
77			type = ((reg >> 16) & 0xff);
(gdb) 
76			cfg = readl(&scu->config) & 3;
(gdb) 
78			if (type == MXC_CPU_MX6DL) {
(gdb) 
83			if (type == MXC_CPU_MX6Q) {
(gdb) 
89		major = ((reg >>  & 0xff);
(gdb) 
90		if ((major >= 1) &&
(gdb) 
67	{
(gdb) 
98		return (type << 12) | (reg + (0x10 * (major + 1)));
(gdb) 
99	}
(gdb) 
get_cpu_rev () at arch/arm/cpu/armv7/mx6/soc.c:69
69		u32 reg = readl(&anatop->digprog_sololite);
(gdb) 
70		u32 type = ((reg >> 16) & 0xff);
(gdb) 
73		if (type != MXC_CPU_MX6SL) {
(gdb) 
74			reg = readl(&anatop->digprog);
(gdb) 
76			cfg = readl(&scu->config) & 3;
(gdb) 
77			type = ((reg >> 16) & 0xff);
(gdb) 
76			cfg = readl(&scu->config) & 3;
(gdb) 
78			if (type == MXC_CPU_MX6DL) {
(gdb) 
83			if (type == MXC_CPU_MX6Q) {
(gdb) 
89		major = ((reg >>  & 0xff);
(gdb) 
90		if ((major >= 1) &&
(gdb) 
67	{
(gdb) 
98		return (type << 12) | (reg + (0x10 * (major + 1)));
(gdb) 
99	}
(gdb) 
get_cpu_rev () at arch/arm/cpu/armv7/mx6/soc.c:69
69		u32 reg = readl(&anatop->digprog_sololite);
(gdb) 
70		u32 type = ((reg >> 16) & 0xff);
(gdb) 
73		if (type != MXC_CPU_MX6SL) {
(gdb) 
74			reg = readl(&anatop->digprog);
(gdb) 
76			cfg = readl(&scu->config) & 3;
(gdb) 
77			type = ((reg >> 16) & 0xff);
(gdb) 
76			cfg = readl(&scu->config) & 3;
(gdb) 
78			if (type == MXC_CPU_MX6DL) {
(gdb) 
83			if (type == MXC_CPU_MX6Q) {
(gdb) 
89		major = ((reg >>  & 0xff);
(gdb) 
90		if ((major >= 1) &&
(gdb) 
67	{
(gdb) 
98		return (type << 12) | (reg + (0x10 * (major + 1)));
(gdb) 
99	}
(gdb) 
lowlevel_init () at arch/arm/cpu/armv7/lowlevel_init.S:69
69		pop	{ip, pc}
(gdb) 
save_boot_params_ret () at arch/arm/cpu/armv7/start.S:88
88		bl	_main
(gdb) 
_main () at arch/arm/lib/crt0.S:76
76		ldr	r0, =(CONFIG_SYS_INIT_SP_ADDR)
(gdb) s
78		bic	r0, r0, #7	/* 8-byte alignment for ABI compliance */
(gdb) 
79		mov	sp, r0
(gdb) 
_main () at arch/arm/lib/crt0.S:80
80		bl	board_init_f_alloc_reserve
(gdb) 
board_init_f_alloc_reserve (top=9568000) at common/init/board_init.c:53
53		top = rounddown(top-sizeof(struct global_data), 16);
(gdb) 
56	}
(gdb) 
_main () at arch/arm/lib/crt0.S:81
81		mov	sp, r0
(gdb) 
_main () at arch/arm/lib/crt0.S:83
83		mov	r9, r0
(gdb) 
84		bl	board_init_f_init_reserve
(gdb) 
board_init_f_init_reserve (base=9566720) at common/init/board_init.c:111
111		memset(gd_ptr, '\0', sizeof(*gd));
(gdb) 
101	{
(gdb) 
111		memset(gd_ptr, '\0', sizeof(*gd));
(gdb) 
memset () at arch/arm/lib/memset.S:24
24		ands	r3, r0, #3		@ 1 unaligned?
(gdb) 
25		mov	ip, r0			@ preserve r0 as return value
(gdb) 
26		bne	6f			@ 1
(gdb) 
30	1:	orr	r1, r1, r1, lsl #8
(gdb) 
31		orr	r1, r1, r1, lsl #16
(gdb) 
32		mov	r3, r1
(gdb) 
33		cmp	r2, #16
(gdb) 
34		blt	4f
(gdb) 
69		stmfd	sp!, {r4-r8, lr}
(gdb) 
memset () at arch/arm/lib/memset.S:70
70		mov	r4, r1
(gdb) 
71		mov	r5, r1
(gdb) 
72		mov	r6, r1
(gdb) 
73		mov	r7, r1
(gdb) 
74		mov	r8, r1
(gdb) 
75		mov	lr, r1
(gdb) 
77		cmp	r2, #96
(gdb) 
78		tstgt	ip, #31
(gdb) 
79		ble	3f
(gdb) 
91	3:	subs	r2, r2, #64
(gdb) 
92		stmiage	ip!, {r1, r3-r8, lr}
(gdb) 
93		stmiage	ip!, {r1, r3-r8, lr}
(gdb) 
94		bgt	3b
(gdb) 
91	3:	subs	r2, r2, #64
(gdb) 
92		stmiage	ip!, {r1, r3-r8, lr}
(gdb) 
93		stmiage	ip!, {r1, r3-r8, lr}
(gdb) 
94		bgt	3b
(gdb) 
91	3:	subs	r2, r2, #64
(gdb) 
92		stmiage	ip!, {r1, r3-r8, lr}
(gdb) 
93		stmiage	ip!, {r1, r3-r8, lr}
(gdb) 
94		bgt	3b
(gdb) 
91	3:	subs	r2, r2, #64
(gdb) 
92		stmiage	ip!, {r1, r3-r8, lr}
(gdb) 
93		stmiage	ip!, {r1, r3-r8, lr}
(gdb) 
94		bgt	3b
(gdb) 
95		ldmfdeq	sp!, {r4-r8, pc}
(gdb) 
97		tst	r2, #32
(gdb) 
98		stmiane	ip!, {r1, r3-r8, lr}
(gdb) 
99		tst	r2, #16
(gdb) 
100		stmiane	ip!, {r4-r7}
(gdb) 
101		ldmfd	sp!, {r4-r8, lr}
(gdb) 
memset () at arch/arm/lib/memset.S:105
105	4:	tst	r2, #8
(gdb) 
106		stmiane	ip!, {r1, r3}
(gdb) 
107		tst	r2, #4
(gdb) 
108		strne	r1, [ip], #4
(gdb) 
113	5:	tst	r2, #2
(gdb) 



114		strbne	r1, [ip], #1
(gdb) 




115		strbne	r1, [ip], #1
(gdb) 
116		tst	r2, #1
(gdb) 
117		strbne	r1, [ip], #1
(gdb) 
118		ret	lr
(gdb) 
board_init_f_init_reserve (base=9566720) at common/init/board_init.c:117
117		base += roundup(sizeof(struct global_data), 16);
(gdb) 
126		gd->malloc_base = base;
(gdb) 
130	}
(gdb) 
_main () at arch/arm/lib/crt0.S:86
86		mov	r0, #0
(gdb) 
87		bl	board_init_f
(gdb) 
board_init_f (boot_flags=0) at common/board_f.c:930
930		gd->have_console = 0;
(gdb) 
929		gd->flags = boot_flags;
(gdb) 
932		if (initcall_run_list(init_sequence_f))
(gdb) 
930		gd->have_console = 0;
(gdb) 
932		if (initcall_run_list(init_sequence_f))
(gdb) 
initcall_run_list (init_sequence=init_sequence@entry=0x87870048 <init_sequence_f>) at lib/initcall.c:17
17		for (init_fnc_ptr = init_sequence; *init_fnc_ptr; ++init_fnc_ptr) {
(gdb) 
14	{
(gdb) 
17		for (init_fnc_ptr = init_sequence; *init_fnc_ptr; ++init_fnc_ptr) {
(gdb) 
21			if (gd->flags & GD_FLG_RELOC)
(gdb) 
22				reloc_ofs = gd->reloc_off;
(gdb) 
27			if (gd->flags & GD_FLG_RELOC)
(gdb) 
31			ret = (*init_fnc_ptr)();
(gdb) 

^C
Program received signal SIGTRAP, Trace/breakpoint trap.
0xdeadbeee in ?? ()
(gdb) s
Cannot find bounds of current function
(gdb) s
Cannot find bounds of current function
(gdb) 

So yeah, technically, I am able to debug U-boot but unable to pass first initialization procedures until any log message. But I am pretty sure that U-boot is correct as I am using it for a while!

Any ideas what is wrong?

 

0 件の賞賛
返信

11,279件の閲覧回数
Almaz
Contributor I

Then I did following:

(gdb) load
Loading section .text, size 0x67458 lma 0x87800000
Loading section .rodata, size 0x14246 lma 0x87867458
Loading section .hash, size 0x18 lma 0x8787b6a0
Loading section .data, size 0x6ca4 lma 0x8787b6b8
Loading section .got.plt, size 0xc lma 0x8788235c
Loading section .u_boot_list, size 0x1208 lma 0x87882368
Loading section .efi_runtime, size 0x100 lma 0x87883570
Loading section .efi_runtime_rel, size 0x90 lma 0x87883670
Loading section .rel.dyn, size 0xd220 lma 0x87883700
Loading section .dynsym, size 0x30 lma 0x87890920
Loading section .dynstr, size 0x1 lma 0x87890950
Loading section .dynamic, size 0x90 lma 0x87890954
Loading section .gnu.hash, size 0x18 lma 0x878909e4
Start address 0x87800000, load size 592375
Transfer rate: 69 KB/sec, 12341 bytes/write.
(gdb) s
reset () at arch/arm/cpu/armv7/start.S:40
40		b	save_boot_params
(gdb) delete
(gdb) b initcall_run_list
Breakpoint 1 at 0x87856dec: file lib/initcall.c, line 17.
(gdb) s
save_boot_params () at arch/arm/cpu/armv7/start.S:116
116		b	save_boot_params_ret		@ back to my caller
(gdb) c
Continuing.

Breakpoint 1, initcall_run_list (init_sequence=init_sequence@entry=0x87870048 <init_sequence_f>) at lib/initcall.c:17
17		for (init_fnc_ptr = init_sequence; *init_fnc_ptr; ++init_fnc_ptr) {

and yeah, I definitely debugging something but it fails on the early steps. Still can't understand what is wrong.

0 件の賞賛
返信

11,270件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Almaz

 

suggest to post on segger forum.

 

Best regards
igor

0 件の賞賛
返信

11,090件の閲覧回数
Almaz
Contributor I

Got it working. Prepared Docker image to get things easier. Thank you very much for your help!

0 件の賞賛
返信