Debugging Linux Kernel on IMx6SoloX through Lauterbach Debugger

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Debugging Linux Kernel on IMx6SoloX through Lauterbach Debugger

2,585 次查看
niranjanbc
Contributor IV

Hi 

 

I am trying to debug the Linux Kernel running on IMX6SoloX with Lauterbach, but my Linux never boots up.

attached is the script file, i am using to initialize the board and load Kernel, DTB & Ram Disk. I am not sure weather i am loading those at right address, where and how do i find those values from.

 

From Script file, i have some comments below. can someone correct me if i am wrong. suggest where i can find the right values.

 

199852_199852.pngpastedImage_1.png

199895_199895.pngpastedImage_2.png

 

 

Thanks

Niranjan

Original Attachment has been moved to: imx6solox_linux_ph_att.cmm.zip

0 项奖励
回复
2 回复数

2,278 次查看
Yuri
NXP Employee
NXP Employee

Hello,

 Please create request in order to send You some Linux (JTAG based) debug considerations.

Support|NXP 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,278 次查看
niranjanbc
Contributor IV

Thank Yuri 

will do

0 项奖励
回复