IMXAI2ETH-BRC and mpc5604E KIT schematics

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMXAI2ETH-BRC and mpc5604E KIT schematics

1,328件の閲覧回数
mo_nas
Contributor I

Good Day,

im Working with the Board SABRE 2 (MCIMX6QAICPU2) and i need the schematic for the daughter board IMXAI2ETH-BRC and for the camera kit mpc5604E KIT. Can someone please share the schematics? Thanks.

ラベル(3)
4 返答(返信)

914件の閲覧回数
wajdidarmoul
Contributor I

Hello I also need schematic SCH-27954 of Broadcom
Ethernet PHY Card - RGMII
Schematic SCH-27954
Part No. IMXAI2ETH-BRC

where to download?

0 件の賞賛
返信

914件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

Schematics for the camera kit are located here:

NXP MPC5604EKIT:Development Kit|NXP

914件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

You can download the schematics for the IMXAI2ETH-BRC in the following link:

SABRE-2|Automotive-Infotainment|i.MX6|NXP

914件の閲覧回数
mo_nas
Contributor I

Hello SergioSolis,

Thank you for sharing the links.

i could find the schematics for the camera-Kit in the link, which you posted.

But i cant find the schematic for MXAI2ETH-BRC in the link https://community.freescale.com/external-link.jspa?url=http%3A%2F%2Fwww.nxp.com%2Fproducts%2Fmicroco...

There are the schematic for the SABRE-Boards and just for the daughter card IMXAI2ETH-ATH. But not the schematics for IMXAI2ETH-BRC (SCH-27954). DO you have a link for the right (BRC) card?

0 件の賞賛
返信