Debugging Cortex-M4 core on i.MX7ULP-EVK on a Linux host

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Debugging Cortex-M4 core on i.MX7ULP-EVK on a Linux host

1,726 次查看
lorv
Contributor III

I have an EVK-MCIMX7ULP eval board and have installed the SDK_2_9_0_EVK-MCIMX7ULP for GCC toolchain. I managed to build several demo applications and load them to QSPI-flash according to this guide.

However I have not found a way to debug code on the Cortex-M4 form my Linux host. The "Getting Started with MCUXpresso SDK for EVK-MCIMX7ULP" only describes debugging using the IAR, which is not available for Linux.

The debug probe I am using is a Segger J-link EDU.

I have tried getting it to work with the help of these posts:

1: Debugging Cortex-M4 on i.MX7D with Segger J-Link and GDB (and thus standard Eclipse) 

2: Debugging MIMXRT1020 with Segger Ozone 

But neither is for the i.MX7ULP processor and I could not manage to get it to work. I guess the instructions in 1) would work for the i.MX7ULP with some changes, but I have never worked with plain eclipse and the instruction are therefore a bit cryptic to me.

I don't really care what debugger to use but if someone could provide some instructions what I have to do to debug on the Cortex-M4 on the i.MX7ULP board that would be highly appreciated.

Best regards,

David

 

 

0 项奖励
回复
4 回复数

1,721 次查看
igorpadykov
NXP Employee
NXP Employee

Hi David

 

one can try lauterbach tools available on linux

https://www.lauterbach.com/frames.html?home.html

 

1.jpg

 

Best regards
igor

 

Best regards
igor

0 项奖励
回复

1,717 次查看
lorv
Contributor III

Hi Igor,

thanks for coming back to me so fast.

It seems to me that with Lauterbach I would need one of their debug probes.

I would like to use my Segger J-link probe that I already have. Is there no possibility to get that to work?

Best regards,

David

0 项奖励
回复

1,710 次查看
igorpadykov
NXP Employee
NXP Employee

Hi David

 

I am afraid Segger J-link probe will not work.

For Segger with LInux one can look below link

https://www.segger.com/products/development-tools/embedded-studio/

 

Best regards
igor

0 项奖励
回复

1,690 次查看
lorv
Contributor III

Hi Igor,

The SDK I downloaded is for GCC toolchain.
As far as I know Segger Embedded Studio is not supported in the SDK. Please correct me If I am wrong.

I would consider using Segger Embedded studio to debug the M4-core if that is possible.

However I would need a little more guidance from you on how to set this up.

Thanks for you help.

Best David

0 项奖励
回复