While debugging i got the problem
Probe Firmware: MCU-LINK on-board (r0E2) CMSIS-DAP V2.250 (NXP Semiconductors)
Serial Number: NVUYDXEI5YUN1
VID:PID: 1FC9:0143
USB Path: \\?\hid#vid_1fc9&pid_0143&mi_00#7&38ddcd02&0&0000#{4d1e55b2-f16f-11cf-88cb-001111000030}
connection failed - Em(04). Cannot provide power to DAP bus... Retrying
Failed on connect: Em(04). Cannot provide power to DAP bus.
Connected&Reset. Was: NotConnected. DpID: 6BA02477. CpuID: 00000000. Info: <None>
Last stub error 0: OK
Last sticky error: 0x0 AIndex: 0
No debug bus (MemAp) selected
DAP Speed test unexecuted or failed
Debug protocol: SWD. RTCK: Disabled. Vector catch: Disabled
How can I solve it?? Pl guide me
解決済! 解決策の投稿を見る。
Hi @KKR231 ,
Thanks for your updated information.
Please follow me:
1. Board power off, then SW1 : 1-off,2-off,3-off,4-on
2. Find another USB cable, connect to the J20
3. power on the board.
4. open the MCUbootutility tool:
https://github.com/JayHeng/NXP-MCUBootUtility/releases/tag/v6.2.0
the related user manual is:
https://github.com/JayHeng/NXP-MCUBootUtility
Use the mcubootutility to do the mass erase:
After the erase finished, then can switch the SW1 back to internal boot mode, SW1:1-OFF,2-OFF,3-ON, 4-OFF, then use the on board CMSIS DAP download the code in the mcuxpresso IDE again.
Please try it.
If you still have question about it, please kindly let me know.
Best Regards,
kerry
Hi @KKR231 ,
Thank you for your interest in the NXP MIMXRT product, I would like to provide service for you.
Whether you can do the CMSIS DAP debug in the MIMXRT1170-EVKB previously?
Do you update the CMSIS DAP version or not recently?
I think your situation may related to the following 2 points:
1. You may download some abnormal app to the flash, that will cause the debugger connection issues, you can refer to my document:
2. If you update the CMSIS DAP version
You can power on the board with the external DC power supply, or you also can find anoter USB cable to connect the SDP USB interface to power on it.
As I know, new CMSIS DAP have the power on issues, need to use ansother USB or the DC power to power on the board.
Please try it on your side.
If you still have question about ti, please kindly let me know.
Best Regards,
Kerry
Still i got following problem during flashing RT
"Executing flash operation 'Erase' (Erase flash) - Mon Jul 08 09:37:17 IST 2024
Checking MCU info...
Scanning for targets...
Executing flash action...
MCUXpresso IDE RedlinkMulti Driver v11.9 (Dec 11 2023 18:02:10 - crt_emu_cm_redlink.exe build 2)
( 0) Reading remote configuration
Found chip XML file in C:/Users/Admin/Documents/MCUXpressoIDE_11.9.0_2144/workspace/FreeRTOS_TAD_logs/evkbmimxrt1170_iled_blinky_cm4/Debug\MIMXRT1176xxxxx.xml
( 5) Remote configuration complete
Reconnected to existing LinkServer process.
============= SCRIPT: RT1170_connect_M7_wake_M4.scp =============
RT1170 Connect M7 and Wake M4 Script
DpID = 6BA02477
Error: No power acknowledge on DAP bus
Setting M4 spin code
Error: Wire Ack Fault - target connected?
Error: Wire Ack Fault - target connected?
Error: Wire Ack Fault - target connected?
Error: Wire Ack Fault - target connected?
Setting M4 clock
Error: Wire Ack Fault - target connected?
Resetting M4 core
Error: Wire Ack Fault - target connected?
Error: Wire Ack Fault - target connected?
Error: Wire Ack Fault - target connected?
Error: Wire Ack Fault - target connected?
Error: Wire Ack Fault - target connected?
View cores on the DAP AP
DpID = 6BA02477
Error: Wire Ack Fault - target connected?
Error: Wire Ack Fault - target connected?
============= END SCRIPT ========================================
Probe Firmware: MCU-LINK on-board (r0E2) CMSIS-DAP V2.250 (NXP Semiconductors)
Serial Number: NVUYDXEI5YUN1
VID:PID: 1FC9:0143
USB Path: \\?\hid#vid_1fc9&pid_0143&mi_00#7&38ddcd02&0&0000#{4d1e55b2-f16f-11cf-88cb-001111000030}
connection failed - Em(04). Cannot provide power to DAP bus... Retrying
Failed on connect: Em(04). Cannot provide power to DAP bus.
Connected&Reset. Was: NotConnected. DpID: 6BA02477. CpuID: 00000000. Info: <None>
Last stub error 0: OK
Last sticky error: 0x0 AIndex: 0
No debug bus (MemAp) selected
DAP Speed test unexecuted or failed
Debug protocol: SWD. RTCK: Disabled. Vector catch: Disabled.
(100) Target Operation Failed
Unable to perform operation!
Command failed with exit code 1"
I set SW1 in serial mode but it's not working.
Hi @KKR231 ,
Thanks for your updated information.
Please follow me:
1. Board power off, then SW1 : 1-off,2-off,3-off,4-on
2. Find another USB cable, connect to the J20
3. power on the board.
4. open the MCUbootutility tool:
https://github.com/JayHeng/NXP-MCUBootUtility/releases/tag/v6.2.0
the related user manual is:
https://github.com/JayHeng/NXP-MCUBootUtility
Use the mcubootutility to do the mass erase:
After the erase finished, then can switch the SW1 back to internal boot mode, SW1:1-OFF,2-OFF,3-ON, 4-OFF, then use the on board CMSIS DAP download the code in the mcuxpresso IDE again.
Please try it.
If you still have question about it, please kindly let me know.
Best Regards,
kerry