IMX93 USB OTG VBUS Error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX93 USB OTG VBUS Error

4,105件の閲覧回数
AlanWen
Contributor IV

Hi,

I'm trying to configure my custom i.MX93 board to switch USB roles from host mode to peripheral. As the custom board setting, USB type-A is for host and a micro USB is for devcie (peripheral).

I'm currently running a custom Linux build based on imx-6.6.3 yocto project

As I modprobe the module g_mass_storage and setup the usb role from host to device, there are some error messages occurred.

root@imx93evk:~# echo host > /sys/bus/platform/devices/ci_hdrc.0/usb_role/ci_hdrc.0-role-switch/role
[   79.667113] ci_hdrc ci_hdrc.0: EHCI Host Controller
root@imx93evk:~# [   79.672827] ci_hdrc ci_hdrc.0: new USB bus registered, assigned bus number 2
[   79.700263] ci_hdrc ci_hdrc.0: USB 2.0 started, EHCI 1.00
[   79.706898] hub 2-0:1.0: USB hub found
[   79.713134] hub 2-0:1.0: 1 port detected

root@imx93evk:~# lsusb
Bus 001 Device 002: ID 05e3:0610 Genesys Logic, Inc. Hub
Bus 001 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub
Bus 002 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub
root@imx93evk:~# modprobe g_mass_storage file=/dev/mmcblk0 removable=1
[  118.913030] Mass Storage Function, version: 2009/09/11
[  118.918280] LUN: removable file: (no medium)
[  118.922669] LUN: removable file: /dev/mmcblk0
[  118.927056] Number of LUNs=1
[  118.930068] g_mass_storage gadget.0: Mass Storage Gadget, version: 2009/09/11
[  118.937246] g_mass_storage gadget.0: userspace failed to provide iSerialNumber
[  118.944532] g_mass_storage gadget.0: g_mass_storage ready
root@imx93evk:~# echo device > /sys/bus/platform/devices/ci_hdrc.0/usb_role/ci_hdrc.0-role-switch/role
[  126.608591] ci_hdrc ci_hdrc.0: remove, state 4
[  126.613071] usb usb2: USB disconnect, device number 1
[  126.620568] ci_hdrc ci_hdrc.0: USB bus 2 deregistered
[  126.626743] usbmisc_imx 4c100200.usbmisc: vbus is error
root@imx93evk:~# [  126.636382] usbmisc_imx 4c100200.usbmisc: Error occurs during detection: -22

 

Here is my kernel device tree setup:

&usbotg1 {
	dr_mode = "otg";
	hnp-disable;
	srp-disable;
	adp-disable;
	usb-role-switch;
	role-switch-default-mode = "host";
	disable-over-current;
	samsung,picophy-pre-emp-curr-control = <3>;
	samsung,picophy-dc-vol-level-adjust = <7>;
	status = "okay";
};

 

Can you help me figure out my issue ?

Sincerely.

タグ(4)
0 件の賞賛
返信
3 返答(返信)

4,097件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

How about your hardware design for the usb1 only support host or dual role?

0 件の賞賛
返信

4,094件の閲覧回数
AlanWen
Contributor IV

A switch controled the USB data bus flow between USB type-A (host) and micro USB (device).

The USB_ID pin only passed through from i.MX93 to micro USB.

For the testing step, maybe I can try the peripheral mode first to connect the PC as device  successfully.

0 件の賞賛
返信

4,046件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Yes, you can try it. If still not work, let us know.

0 件の賞賛
返信