Dead lock occurred while opening /dev/console with ttymxc0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Dead lock occurred while opening /dev/console with ttymxc0

2,191 Views
zhb1984
Contributor I

Hello,

I am using i.MX6SoloX to develop application with custom board.  U-Boot and Linux porting have been done.  Everything is OK except that Linux hung while opening /dev/console with ttymxc0.  It tried to do spin_lock_irqsave in imx_uart_startup.  But at this point, the lock was already acquired.  So dead lock occurred.

Can someone give any advice?

Thanks

Labels (2)
0 Kudos
Reply
3 Replies

2,181 Views
joanxie
NXP TechSupport
NXP TechSupport

for your customized board, did your HW is the same as nxp board? did you use the same uart console as nxp board?

0 Kudos
Reply

2,179 Views
zhb1984
Contributor I

Yes, my board is referenced to Sabre SD board.  But there is no SN74LVC2G126 between i.MX6SX UART and USB bridge.  And UART1 is used as the I/O port which is same as NXP board.

0 Kudos
Reply

2,160 Views
joanxie
NXP TechSupport
NXP TechSupport

try to refer to the enclosed file

0 Kudos
Reply