I forgot to provide 3.3V power to NVCC_ENET, but the external RMII interface PHY chip can work normally. After testing, it is found that the power supply of NVCC_ENET is back-filled to it by the MDIO signal from a pull-up (pull-up resistor of 4.7k) to 3.3V, and it is stable at about 2.140V. When I tried to change 4.7K to 2.2K, I found that the voltage of NVCC_ENET increased to 2.42V,
The first question, I would like to ask why the external 3.3V can be fed back to NVCC_ENET through the MDIO signal?
The second question is, can the risk caused by design problems be reduced to zero by reducing the MDIO pull-up resistance without changing the board?
MCIMX6Q5EYM10AD
@qumai
Hello,
for i.MX6, in any case, NVCC_ENET must be applied.
Customers can refer to Table 2-21 (Recommended connections
for unused analog interfaces) of the Hardware Development Guide.
ENET signals are not mentioned there, assuming NVCC_ENET must
be applied.
http://cache.nxp.com/assets/documents/data/en/user-guides/IMX6DQ6SDLHDG.pdf
Regards,
Yuri.
why the external 3.3V can be fed back to NVCC_ENET through the MDIO signal?
@qumai
Hello,
one of the reasons why all i.MX6 supply voltages should be applied
is leakages avoiding .
Regards,
Yuri.