Hi,
I am trying to load the kernel using uboot and I get a data abort exception. I have followed the procedures same as what is given by Freescale. uboot version : uboot-imx-rel_imx_3.10.53_1.1.1
I have tried putting $(PF_NO_ALIGNED) in the config.mk of the uboot but there is no luck. How can I debug this?
I get the following message:
Normal Boot
Hit any key to stop autoboot: 0
reading uImage
4659752 bytes read in 225 ms (19.8 MiB/s)
reading imx6dl-sabresd.dtb
49157 bytes read in 19 ms (2.5 MiB/s)
## Booting kernel from Legacy Image at 12000000 ...
Image Name: Linux-3.10.53
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 4659688 Bytes = 4.4 MiB
Load Address: 10008000
Entry Point: 10008000
Verifying Checksum ... OK
## Flattened Device Tree blob at 18000000
Booting using the fdt blob at 0x18000000
Loading Kernel Image ... OK
Using Device Tree in place at 18000000, end 1800f004
switch to ldo_bypass mode!
Starting kernel ...
data abort
pc : [<10815be8>] lr : [<10815460>]
sp : 10c87540 ip : 0000001c fp : 10c86540
r10: 10814310 r9 : 10814cd8 r8 : 18000000
r7 : 00000f8c r6 : 10c8654c r5 : 108161fc r4 : 00000055
r3 : 00000f8c r2 : f42ec000 r1 : 021ec000 r0 : 00000055
Flags: nzCv IRQs off FIQs off Mode SVC_32
Resetting CPU ...
resetting ...
My fdt_addr is 0x18000000
and my loadaddr is 0x12000000
What seems to have gone wrong? I have booted this properly with one set of boards where the UART was uart3. The newer boards have UART as UART1 and that is the only change done. Also I find that exception happens when the kernel entry point function pointer gets called in uboot.