DSP can't ouput debug log on IMX8MP

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

DSP can't ouput debug log on IMX8MP

1,526 次查看
jimmyli
Contributor IV

Hi,

      We are trying to run HIFI4 dsp on IMX8MP, but encounter a question shown as below:

      1>Linux version:  L5.10.72-2.2.2

      2>We do as 《i.MX DSP User's Guide》chapter 4.3, but uart4 can't output the log message.

          Only in kernel, we can output the log message from uart4, the harware is ok.

     

       Can you help to check and fix it?

       Thanks very much.

----log screen shot.

jimmyli_0-1683169176524.png

 

标签 (1)
0 项奖励
回复
4 回复数

1,471 次查看
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @jimmyli,

I hope you are doing well.

UART4 is used for Cortex-M7 core.
Disable UART4 in Linux OS & M7 core as DSP firmware runs on HiFi core.
In ATF, UART4 should be allocated to hifi4 core using RDC. 

Thanks & Regards,
Sanket Parekh
0 项奖励
回复

1,467 次查看
jimmyli
Contributor IV

Hi Dhruvit,

     Got it.

      Thanks very much.

0 项奖励
回复

1,401 次查看
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hello @jimmyli 

I hope you are doing well.

I'm glad to help you, if the issue is solved, can I close the thread?

Thanks & Regards,

Sanket Parekh

0 项奖励
回复

1,366 次查看
jimmyli
Contributor IV

Hi Sanket,

       Sorry for replying too late.

       Yes, we have resolve the problem.

 

      Thanks very much.

标记 (1)
0 项奖励
回复