MCIMX93-EVKCM About the eIQ demo at yocto

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCIMX93-EVKCM About the eIQ demo at yocto

Jump to solution
849 Views
Ryo_Aoki
Contributor III

Hi community.

I want to demo eIQ using MCIMX93-EVKCM.

(about MACHINE LEARNING UG  11.2 TensorFlow Lite Demos for i.MX 93)

A demo image is created with reference to the following document.

  ..i.MX Machine Learning User's Guide Rev. LF6.1.1_1.0.0 — 31 March 2023

  ..i.MX Yocto Project User's Guide Rev. LF6.1.1_1.0.0 — 24 April 2023

 

But i can't run the demo because there is a problem with file reference.

The image was created using the following procedure.

 

$ repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-langdale -m imx-6.1.1-1.0.0.xml

$ repo sync

$ DISTRO=fsl-imx-xwayland MACHINE=imx93evk source imx-setup-release.sh -b build-93evk

 Add the following to local.conf

  IMAGE_INSTALL:append = " python3-git python3-wheel“

  IMAGE_INSTALL:append = " tensorflow-lite-ethosu-delegate“

  TOOLCHAIN_TARGET_TASK:append = “ tensorflow-lite-dev onnxruntime-dev” 

$ bitbake imx-image-full

 

The manual says /usr/bin/eiq-examples-git exists.

But the eiq-examples-git folder exists only in /run/media/root-mmcblk1p2/usr/bin/.

I think that it is necessary to correct the reference destination of the library and the module if this folder structure is left as it is.

Is there anything I need to do to make it work as documented?

 

Paste the result of the df command.

Filesystem 1K-blocks Used Available Use% Mounted on
/dev/root 3398680 1682604 1520156 53% /
devtmpfs 733836 4 733832 1% /dev
tmpfs 997452 0 997452 0% /dev/shm
tmpfs 398984 10256 388728 3% /run
tmpfs 4096 0 4096 0% /sys/fs/cgroup
tmpfs 997452 12 997440 1% /tmp
tmpfs 997452 164 997288 1% /var/volatile
tmpfs 199488 4 199484 1% /run/user/0
/dev/mmcblk0p1 84998 31770 53228 38% /run/media/boot-mmcblk0p1
/dev/mmcblk1p1 84998 32926 52072 39% /run/media/boot-mmcblk1p1
/dev/mmcblk1p2 11652524 2996176 8033000 28% /run/media/root-mmcblk1p2

 

Best regards.

Tags (1)
0 Kudos
Reply
1 Solution
766 Views
Ryo_Aoki
Contributor III

Hi Joan.

This issue is probably resolved.

The cause was a mistake in the boot mode, and it was booting from a different place than expected.

After correcting the boot settings, the eiq sample folder existed in the expected folder.

Sorry for the cheap mistake.This thread will be closed.

thank you for your support.

 

Best regards.

View solution in original post

0 Kudos
Reply
3 Replies
823 Views
joanxie
NXP TechSupport
NXP TechSupport

I haven't built this image for eIQ, let me reproduce this and tell you the result

0 Kudos
Reply
767 Views
Ryo_Aoki
Contributor III

Hi Joan.

This issue is probably resolved.

The cause was a mistake in the boot mode, and it was booting from a different place than expected.

After correcting the boot settings, the eiq sample folder existed in the expected folder.

Sorry for the cheap mistake.This thread will be closed.

thank you for your support.

 

Best regards.

0 Kudos
Reply
799 Views
Ryo_Aoki
Contributor III

Hi Joan.
Thanks your reply.

I created the image with reference to the documentation,
but any help on how to fix it would be appreciated.

0 Kudos
Reply