DIP Switch Overrides

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DIP Switch Overrides

3,870 Views
pilotnite
Contributor III

Support,

We are currently working on a project where we need to change the boot media from eMMC to SPI flash. However, physically accessing the hardware to adjust DIP switch settings is not feasible in our situation.

Is there any way to change the boot media via software, specifically using the uuu utility, by burning fuses that would override the DIP switch settings? We are interested in a solution that avoids the need for physical changes to the hardware.

Any guidance or recommendations would be greatly appreciated.

Thank you for your assistance.

Tags (1)
0 Kudos
Reply
7 Replies

3,835 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

It is need hardware to change boot mode. If your board is not flashed, it will go automatically to serial download mode. Then you can configure fuses and do a permanent change in fuses to SPI flash.

Best regards.

0 Kudos
Reply

3,827 Views
pilotnite
Contributor III

@JorgeCas 

Thanks for your feedback.

Can you please elaborate more on how to configure the fuses? 

0 Kudos
Reply

3,825 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Sure, I suggest you take a look in the next link.

Best regards.

0 Kudos
Reply

3,823 Views
pilotnite
Contributor III

@JorgeCas 

Thanks for the link. Is this same for i.mx93? 

0 Kudos
Reply

3,819 Views
pilotnite
Contributor III

@JorgeCas 

Just to reiterate, I'm looking for instructions for i.mx93, on how to set boot mode to SPI boot from eMMC without changing DIP switches. 

0 Kudos
Reply

3,820 Views
JorgeCas
NXP TechSupport
NXP TechSupport

I apologize, I got confused with the label in your post.

JorgeCas_0-1727722865181.png

 

 

It is similar, it does not use SCFW API functions and fuses arrays are different. Programing eFuses using U-Boot is the same.

Please check this link.

Best regards.

0 Kudos
Reply

3,791 Views
pilotnite
Contributor III

@JorgeCas 

Thank you for your feedback and for sharing the link.

I’m still working to find the best solution and want to avoid any risk of bricking the devices during the process. Is there any way you can assist in determining the correct fuse to burn in order to achieve the desired setup?

Specifically, for the i.MX93, I need to change the boot media from eMMC to SPI. Can this be done through U-Boot or the uuu utility? If so, could you please provide the exact commands and values needed to implement this change?

I appreciate your help and guidance.

Tags (1)
0 Kudos
Reply