DHCP Server in IMX RT 1170 using Lwip stack

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DHCP Server in IMX RT 1170 using Lwip stack

2,421件の閲覧回数
Febin
Contributor I

Hi

My board has an IMXRT1170 processor and Wifi chip from Ti and runs on FreeRTOS and lwip stack. I'm trying to integrate a dhcp server in Wifi AP mode. I have tested the dhcp server code which uses Lwip in ethernet medium in IMX RT 1050 and its working fine. My laptop is able to get a dynamic address.

But in wifi, the board is receiving DHCP_DISCOVER and sending a DHCP_OFFER response. But the client is not receiving the DHCP_OFFER message or a dynamic address. The DHCP offer message contains a valid ip address offered. I am attaching wireshark dump. 

What could be the reason DHCP_OFFER is not accepted by client?

 

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

2,397件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi Febin:

 

Since Ethernet medium can work and WIFI not, I would suggest you post this question on TI WIFI community to get fast help.

https://www.ti.com/wireless-connectivity/wi-fi/overview.html

 

Regards

Daniel

 

タグ(1)
0 件の賞賛
返信