DDR3 Write Leveling

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DDR3 Write Leveling

3,138件の閲覧回数
tony_l_cai
Contributor III

Dear All,

     What the conditions will we use the DDR3 Write Leveling features?we dont know why we need to fix the following Data pin ,in other word, D0 is connected to DRAM_D8 not DRAM_D0.

FSL review command as below:

==============================================================

The review was finished. One comment about DDR3 data swapping of the review,

Hardware write leveling – lowest order bit within byte lane must remain on lowest order bit of lane

by JEDEC compliance (see the “Write Leveling” section in JESD79-3E)

D0, D8, D16, D24, D32, D40, D48, and D56 are fixed

Other data lines free to swap within byte lane

For example, DQ0 of U3 should connect to net-label DRAM_D8.

ラベル(2)
0 件の賞賛
返信
1 返信

2,466件の閲覧回数
Yuri
NXP Employee
NXP Employee

   Please look at section 11 (Write Leveling) of app note AN4467.

"i.MX 6 Series DDR Calibration"

http://cache.freescale.com/files/32bit/doc/app_note/AN4467.pdf

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信