DDR test pattern

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DDR test pattern

2,932件の閲覧回数
Kazuma_Sasaki
Senior Contributor I

We are using DDR Stress Test Tool V2.7. as you know, it can be execute stress test via this tool.

Then, I got following log. It seems six or seven test cases executed.

What kind of test executed by this tool? Could you elaborate all test scenarios?

DDR Freq: 396 MHz

t0.1: data is addr test

t0: memcpy10 SSN x64 test

t1: memcpy8 SSN x64 test

t2: byte-wise SSN x64 test

t3: memcpy11 random pattern test

t4: IRAM_to_DDRv2 test

t5: IRAM_to_DDRv1 test

t6: read noise walking ones and zeros test

Best Regards,

Kazuma Sasaki.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,457件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信

2,457件の閲覧回数
Kazuma_Sasaki
Senior Contributor I

Hi,

I have checked these thread. but, it does not mentioned stress test pattern.

Are you able to point out it?

Best Regards,

Kazuma Sasaki.

0 件の賞賛
返信