DDR stress test tool

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,306件の閲覧回数
ioancalapod
Contributor II

Hi All

 

I just ran the DDR Stress test tool.

I got the two files (attached):

ddr_calibration_20150819-11'38'44.log

ddr_stresstest_20150719-12'57'12.log

 

I was wondering if one can recommend a/few document/s to help interpret them in more depth...?

 

Thanks, Ioan

Original Attachment has been moved to: ddr_stresstest_20150719-12'57'12.log.zip

Original Attachment has been moved to: ddr_calibration_20150819-11'38'44.log.zip

ラベル(6)
0 件の賞賛
返信
1 解決策
2,828件の閲覧回数
BiyongSUN
NXP Employee
NXP Employee
0 件の賞賛
返信
2 返答(返信)
2,828件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi ioan

basic principles are described in

Application Note AN4467 (Rev. 0, 10/2012)

"i.MX 6 Series DDR Calibration"

http://www.freescale.com/files/32bit/doc/app_note/AN4467.pdf

Best regards

igor

0 件の賞賛
返信
2,829件の閲覧回数
BiyongSUN
NXP Employee
NXP Employee

i.MX6 DDR Stress Test Tool

https://community.freescale.com/docs/DOC-96412

i.Mx6DQSDL DDR3 Script Aid

https://community.freescale.com/docs/DOC-94917

Freescale i.MX6 DRAM Port Application Guide-DDR3

https://community.freescale.com/docs/DOC-101708

0 件の賞賛
返信