DDR register varification in U-boot for imx6q

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

DDR register varification in U-boot for imx6q

跳至解决方案
1,547 次查看
prathamrahate
Contributor III

I have done calibration using DDR calibration tool on imx6q sabresd board. The results from calibration were different from that mentioned in DCD data in board/freescale/mx6sabresd/mx6q_4x_mt41j128.cfg. Why there is difference ??

标签 (3)
0 项奖励
回复
1 解答
1,354 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Pratham

it was created with older tool versions and works fine as

has sufficient calibration margins.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

3 回复数
1,355 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Pratham

it was created with older tool versions and works fine as

has sufficient calibration margins.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,354 次查看
prathamrahate
Contributor III

Thanks, Igor. I have used v2.52 tool, which is latest. That might be the difference.

0 项奖励
回复
1,354 次查看
Yuri
NXP Employee
NXP Employee

JFYI : v2.60 is the recent.

~Yuri.