DDR register varification in U-boot for imx6q

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR register varification in U-boot for imx6q

Jump to solution
1,549 Views
prathamrahate
Contributor III

I have done calibration using DDR calibration tool on imx6q sabresd board. The results from calibration were different from that mentioned in DCD data in board/freescale/mx6sabresd/mx6q_4x_mt41j128.cfg. Why there is difference ??

Labels (3)
0 Kudos
Reply
1 Solution
1,356 Views
igorpadykov
NXP Employee
NXP Employee

Hi Pratham

it was created with older tool versions and works fine as

has sufficient calibration margins.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

3 Replies
1,357 Views
igorpadykov
NXP Employee
NXP Employee

Hi Pratham

it was created with older tool versions and works fine as

has sufficient calibration margins.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,356 Views
prathamrahate
Contributor III

Thanks, Igor. I have used v2.52 tool, which is latest. That might be the difference.

0 Kudos
Reply
1,356 Views
Yuri
NXP Employee
NXP Employee

JFYI : v2.60 is the recent.

~Yuri.