Hi @logic887,
I hope you are doing well.
From the RPA file, It seems that the DDR clock frequency is changed from the default configuration.
Please note that RPA file only supports 1500Mhz and 2000Mhz clock frequency
For frequencies other than these two, it is up to the user to create the appropriate register setting for the desired frequency. (DRAM_PLL_FDIV_CTL0 ).
Please refer to the below document for more information.
iMX 8M Mini Register Programming Aid DRAM PLL setting
Thanks & Regards,
Dhruvit Vasavada