DDR Tool support for iMX95

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

DDR Tool support for iMX95

跳至解决方案
4,134 次查看
simonng
Contributor III

Hi NXP,

The latest release V3.31 of the DDR Tool has no support of the i.MX95. Is Will this tool include the support of iMX95 in the future?

Thanks.

0 项奖励
回复
1 解答
4,066 次查看
pengyong_zhang
NXP Employee
NXP Employee

Hi @simonng 

Ours is not quite the same. You can try delete the  MIMX95 package in "C:\ProgramData\NXP\mcu_data_v16\processors" directory. And reboot the Config Tool, run the test again.

pengyong_zhang_1-1730859470998.png

B.R

 

 

在原帖中查看解决方案

0 项奖励
回复
9 回复数
3,941 次查看
pengyong_zhang
NXP Employee
NXP Employee

HI @simonng 

Glad to heard this, And for your further another question , i will help you create another ticket talk about it.

B.R

0 项奖励
回复
4,067 次查看
pengyong_zhang
NXP Employee
NXP Employee

Hi @simonng 

Ours is not quite the same. You can try delete the  MIMX95 package in "C:\ProgramData\NXP\mcu_data_v16\processors" directory. And reboot the Config Tool, run the test again.

pengyong_zhang_1-1730859470998.png

B.R

 

 

0 项奖励
回复
3,998 次查看
simonng
Contributor III

Hi @pengyong_zhang ,

I can now run the DDR test with V16.1. Thanks a lot for your help.

Another issue about the DDR data rate setting, there are 4 settings (3200Mbps, 4267Mbps, 4800Mbps and 6400Mbps). Could you give me advice on how to test different frequency other than those 4 templates?

For iMX 8M family, NXP provides the RPA spreadsheet that allow us to update the configurations. Will NXP release it for the iMX95?

Thanks.

0 项奖励
回复
4,082 次查看
pengyong_zhang
NXP Employee
NXP Employee

HI @simonng 

Have you change anything in the DDR Configuration page? You are use our NXP i.MX95 board, right?

And please refer the attachment file.

0 项奖励
回复
4,080 次查看
simonng
Contributor III

Hi @pengyong_zhang ,

I didn't change the LPDDR5 configuration. I am using the NXP IMX95LPDDR5BB-19 EVK board.

I tried to load your ds file but still the same error. Could you help to check my board configuration?

simonng_0-1730858203903.png

 

0 项奖励
回复
4,100 次查看
pengyong_zhang
NXP Employee
NXP Employee

hi @simonng 

Please do not use the old version configuration to the latest version.

Are you sure your Config Tool version is V16.1? Because my v16.1 is different with your ConfigTool_v16_Error.png. Please double check it.

And i run the DDR test on my i.XM95 board, there is no issue occurred.

B.R

0 项奖励
回复
4,084 次查看
simonng
Contributor III

Hi @pengyong_zhang ,

I re-installed V16.1. The error is the same. Please see the attached.

Could you share your config file (.mex) to me?

Thanks.

0 项奖励
回复
4,095 次查看
pengyong_zhang
NXP Employee
NXP Employee

HI @simonng 

You can download our latest DDR Config Tool and run the DDR test about i.MX95.The download link as below:

https://www.nxp.com/design/design-center/development-boards-and-designs/i-mx-evaluation-and-developm...

B.R

0 项奖励
回复
4,093 次查看
simonng
Contributor III

Hi @pengyong_zhang ,

Thanks for your reply. I understand that the Config Tool can support i.MX95.

I can use the REV 15.1 to run the DDR Test on the MX95 EVK board.

But I found problem when using the latest REV 16.1. I tried to load the configuration that I used in REV 15.1. Also, I tried to create new project in REV 16.1. Neither one can work.

I attached the error screenshot.

By the way, I want to know if NXP is going to add the support of i.MX95 to the DDR Tool. 

Thanks for your help.

 

0 项奖励
回复