DDR Tool support for iMX95

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DDR Tool support for iMX95

ソリューションへジャンプ
3,867件の閲覧回数
simonng
Contributor III

Hi NXP,

The latest release V3.31 of the DDR Tool has no support of the i.MX95. Is Will this tool include the support of iMX95 in the future?

Thanks.

0 件の賞賛
返信
1 解決策
3,799件の閲覧回数
pengyong_zhang
NXP Employee
NXP Employee

Hi @simonng 

Ours is not quite the same. You can try delete the  MIMX95 package in "C:\ProgramData\NXP\mcu_data_v16\processors" directory. And reboot the Config Tool, run the test again.

pengyong_zhang_1-1730859470998.png

B.R

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
9 返答(返信)
3,674件の閲覧回数
pengyong_zhang
NXP Employee
NXP Employee

HI @simonng 

Glad to heard this, And for your further another question , i will help you create another ticket talk about it.

B.R

0 件の賞賛
返信
3,800件の閲覧回数
pengyong_zhang
NXP Employee
NXP Employee

Hi @simonng 

Ours is not quite the same. You can try delete the  MIMX95 package in "C:\ProgramData\NXP\mcu_data_v16\processors" directory. And reboot the Config Tool, run the test again.

pengyong_zhang_1-1730859470998.png

B.R

 

 

0 件の賞賛
返信
3,731件の閲覧回数
simonng
Contributor III

Hi @pengyong_zhang ,

I can now run the DDR test with V16.1. Thanks a lot for your help.

Another issue about the DDR data rate setting, there are 4 settings (3200Mbps, 4267Mbps, 4800Mbps and 6400Mbps). Could you give me advice on how to test different frequency other than those 4 templates?

For iMX 8M family, NXP provides the RPA spreadsheet that allow us to update the configurations. Will NXP release it for the iMX95?

Thanks.

0 件の賞賛
返信
3,815件の閲覧回数
pengyong_zhang
NXP Employee
NXP Employee

HI @simonng 

Have you change anything in the DDR Configuration page? You are use our NXP i.MX95 board, right?

And please refer the attachment file.

0 件の賞賛
返信
3,813件の閲覧回数
simonng
Contributor III

Hi @pengyong_zhang ,

I didn't change the LPDDR5 configuration. I am using the NXP IMX95LPDDR5BB-19 EVK board.

I tried to load your ds file but still the same error. Could you help to check my board configuration?

simonng_0-1730858203903.png

 

0 件の賞賛
返信
3,833件の閲覧回数
pengyong_zhang
NXP Employee
NXP Employee

hi @simonng 

Please do not use the old version configuration to the latest version.

Are you sure your Config Tool version is V16.1? Because my v16.1 is different with your ConfigTool_v16_Error.png. Please double check it.

And i run the DDR test on my i.XM95 board, there is no issue occurred.

B.R

0 件の賞賛
返信
3,817件の閲覧回数
simonng
Contributor III

Hi @pengyong_zhang ,

I re-installed V16.1. The error is the same. Please see the attached.

Could you share your config file (.mex) to me?

Thanks.

0 件の賞賛
返信
3,828件の閲覧回数
pengyong_zhang
NXP Employee
NXP Employee

HI @simonng 

You can download our latest DDR Config Tool and run the DDR test about i.MX95.The download link as below:

https://www.nxp.com/design/design-center/development-boards-and-designs/i-mx-evaluation-and-developm...

B.R

0 件の賞賛
返信
3,826件の閲覧回数
simonng
Contributor III

Hi @pengyong_zhang ,

Thanks for your reply. I understand that the Config Tool can support i.MX95.

I can use the REV 15.1 to run the DDR Test on the MX95 EVK board.

But I found problem when using the latest REV 16.1. I tried to load the configuration that I used in REV 15.1. Also, I tried to create new project in REV 16.1. Neither one can work.

I attached the error screenshot.

By the way, I want to know if NXP is going to add the support of i.MX95 to the DDR Tool. 

Thanks for your help.

 

0 件の賞賛
返信