Hi support,
I am developping a iMX8mm board, when I run the ddr tool V3.20, it hangs below.
My PMIC is PCA9450AHN, and the uart configuration is correct.
How can I debug it?
Thanks.
解決済! 解決策の投稿を見る。
Hi everyone,
This issue is fixed, there is something wrong with our hardware design, which makes the CPU enter TEST MODE.
Many thanks to all your support.
Best wishes.
Hi everyone,
This issue is fixed, there is something wrong with our hardware design, which makes the CPU enter TEST MODE.
Many thanks to all your support.
Best wishes.
The ddr tool firmware default is for i.MX8MM evk lpddr4 + rohm pmic.
If it is a customized board, at least need to configure the pmic pca.
the guide is on the page.
Have you done that in the .ds file, as you said you have read the guide?
As we use the PCA9450 PMIC, should we use different ddr firmware in the ddr tool?
We use the PCA9450 PMIC, and I also add the PMIC configuration in the .ds file as below.
##############step 0.5: configure I2C port IO pads according to your PCB design. #####
########### You can modify the following instructions to adapt to your board PMIC #######
memory set 0x30330214 32 0x00000010 #IOMUXC_SW_MUX_I2C1_SCL
memory set 0x30330218 32 0x00000010 #IOMUXC_SW_MUX_I2C1_SDA
memory set 0x3033047C 32 0x000000C6 #IOMUXC_SW_PAD_I2C1_SCL
memory set 0x30330480 32 0x000000C6 #IOMUXC_SW_PAD_I2C1_SDA
sysparam set pmic_cfg 0x004B
#bit[7:0] = PMIC addr,bit[15:8]=I2C Bus.
#Bus index from 0 ('0' = I2C1, '1' = I2C2, '2' = I2C3, '3' = I2C4)
sysparam set pmic_set 0x2F01
#bit[7:0] = Reg val, bit[15:8]=Reg addr.
#REG(0x2F) = 0x01
sysparam set pmic_set 0x0C02
#REG(0x0C) = 0x02
sysparam set pmic_set 0x171E
#REG(0x17) = 0x1E
sysparam set pmic_set 0x0C00
#REG(0x0C) = 0x00
sysparam set pmic_set 0x2F11
#REG(0x2F)=0x11
The script you have added seems exactly the same as the guide.
You should change to " adapt to your board PMIC"
##############step 0.5: configure I2C port IO pads according to your PCB design. #####
########### You can modify the following instructions to adapt to your board PMIC #######
the guide is just example.
You can follow the guide here:https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Family-DDR-Tool-Release/ta-p/110...
Thanks your reply. Yes, I have read this guide, but it still doesn't work.
Have you give the proper configuration for the ddr you are using?
We use the same LPDDR4 configuration as the NXP EVK refrence board.
And I tried to use 1200M, 400M DDR frequency, but it still hangs as below.
Downloading file 'bin\lpddr4_train1d_string_v201709.bin' ..Done
Downloading file 'bin\lpddr4_train2d_string_v201709.bin' ..Done
Downloading file 'bin\lpddr4_imem_1d_v201709.bin' ..Done
Downloading file 'bin\lpddr4_dmem_1d_v201709.bin' ..Done
Downloading file 'bin\lpddr4_imem_2d_v201709.bin' ..Done
Downloading file 'bin\lpddr4_dmem_2d_v201709.bin' ..Done
Downloading IVT header...Done
Downloading file 'bin\m845s_ddr_stress_test.bin' ...Done
Download is complete
Waiting for the target board boot...
You mean you use the same DDR as our reference board design?
Yes, because I don't have the DDR tool source code, I don't know how to debug it.
What's the problem you met? You can tell more details to us.
The DDR tool always hangs as below.
Downloading file 'bin\lpddr4_train1d_string_v201709.bin' ..Done
Downloading file 'bin\lpddr4_train2d_string_v201709.bin' ..Done
Downloading file 'bin\lpddr4_imem_1d_v201709.bin' ..Done
Downloading file 'bin\lpddr4_dmem_1d_v201709.bin' ..Done
Downloading file 'bin\lpddr4_imem_2d_v201709.bin' ..Done
Downloading file 'bin\lpddr4_dmem_2d_v201709.bin' ..Done
Downloading IVT header...Done
Downloading file 'bin\m845s_ddr_stress_test.bin' ...Done
Download is complete
Waiting for the target board boot...
Download is complete
Waiting for the target board boot...
above, it is only the ddr tool output itself.
It says "Waiting for the target board boot...", because it is waiting on the uart for the board output.
In the tool guide document, there is two keys for ".ds":1. how to configure the uart 2. how to configure the pimc.
It is very to simple to tell the different between the i.MX8MM evk and your board those two keys. then change the ".ds" as you said you have read the guide.
the pmic, you can follow the bsp u-boot spl power init code to set the PCA pmic in ".ds"
Hi Biyong,
I doubt the ddr test program don't run correctly, what's your suggestion to further debug?
After all the bin files are downloaded, which bin will run first? m845s_ddr_stress_test.bin?How to check whether it runs or not?
Downloading file 'bin\lpddr4_train1d_string_v201709.bin' ..Done
Downloading file 'bin\lpddr4_train2d_string_v201709.bin' ..Done
Downloading file 'bin\lpddr4_imem_1d_v201709.bin' ..Done
Downloading file 'bin\lpddr4_dmem_1d_v201709.bin' ..Done
Downloading file 'bin\lpddr4_imem_2d_v201709.bin' ..Done
Downloading file 'bin\lpddr4_dmem_2d_v201709.bin' ..Done
Downloading IVT header...Done
Downloading file 'bin\m845s_ddr_stress_test.bin' ...Done
Download is complete
Thanks. First, I have changed the uart configuration according to our design, second, we use the same PMIC PCA9450 as the EVK board. You mean the example below is not for PCA9450?Then what PMIC is it for?
sysparam set pmic_cfg 0x004B
#bit[7:0] = PMIC addr,bit[15:8]=I2C Bus.
#Bus index from 0 ('0' = I2C1, '1' = I2C2, '2' = I2C3, '3' = I2C4)
sysparam set pmic_set 0x2F01
#bit[7:0] = Reg val, bit[15:8]=Reg addr.
#REG(0x2F) = 0x01
sysparam set pmic_set 0x0C02
#REG(0x0C) = 0x02
sysparam set pmic_set 0x171E
#REG(0x17) = 0x1E
sysparam set pmic_set 0x0C00
#REG(0x0C) = 0x00
sysparam set pmic_set 0x2F11
#REG(0x2F)=0x11
Below is the .ds setting I add for PCA9450 from the spl pmic setting.
sysparam set pmic_cfg 0x0025
#bit[7:0] = PMIC addr,bit[15:8]=I2C Bus.
#Bus index from 0 ('0' = I2C1, '1' = I2C2, '2' = I2C3, '3' = I2C4)
sysparam set pmic_set 0x0C29
#REG(0x0C) = 0x29
sysparam set pmic_set 0x1059
#REG(0x10) = 0x59
sysparam set pmic_set 0x1210
#REG(0x12) = 0x10
sysparam set pmic_set 0x171c
#REG(0x17) = 0x1c
sysparam set pmic_set 0x164a
#REG(0x16) = 0x4a
sysparam set pmic_set 0x22c0
#REG(0x22) = 0xc0
sysparam set pmic_set 0x08a1
#REG(0x08) = 0xa1
I measured the I2C_SCL and I2C_SDA signals, there was no operation on them. I think the ddr tool program hasn't run to the setting for PMIC when hangs.