DDR STRESS TEST STOP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,337件の閲覧回数
897122694
Contributor I

I do the DDR3 STRESS TEST ,there is a problem.The test is stuck in the step but no any error information is prompted.As  is shown in the red box below.

Why this problem happen ,who can help me?

DDR Freq: 365 MHz
t0.1: data is addr test
t0: memcpy10 SSN x64 test
t1: memcpy8 SSN x64 test
t2: byte-wise SSN x64 test
t3: memcpy11 random pattern test

ラベル(1)
0 件の賞賛
返信
1 解決策
3,119件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi CAI

most probably board hangs, one can check with oscilloscope power supplies

and clocks using recommendations in i.MX6 System Development User’s Guide

https://www.nxp.com/docs/en/user-guide/IMX6DQ6SDLHDG.pdf

Also one can try to test with simple ddr_test.c with jtag using bare metal sdk

(zip can be found on https://community.nxp.com/thread/432859 )

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
3,120件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi CAI

most probably board hangs, one can check with oscilloscope power supplies

and clocks using recommendations in i.MX6 System Development User’s Guide

https://www.nxp.com/docs/en/user-guide/IMX6DQ6SDLHDG.pdf

Also one can try to test with simple ddr_test.c with jtag using bare metal sdk

(zip can be found on https://community.nxp.com/thread/432859 )

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,119件の閲覧回数
897122694
Contributor I

问题已解决,是在DDR压力测试过程中,外部给IMX6断电复位导致测试中断,电脑会重新识别USB设备。

0 件の賞賛
返信