DCD (Device Configuration Data) for i.Mx6 QuadCore

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

DCD (Device Configuration Data) for i.Mx6 QuadCore

跳至解决方案
6,915 次查看
maheshkumarkoda
Contributor III

Is it possible to modify DCD (Device Configuration Data)? or DCD is hard coded for internal ROM to boot up?

Customized Hardware board with i.Mx6 Quadcore is used in my project.

Also put some light on how DCD is related to pNOR flash with an example?

Thanks a lot :smileyhappy:

标签 (2)
标记 (3)
0 项奖励
回复
1 解答
5,987 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Mahesh

for parallel NOR it is placed on 0x1000 bytes offset and described in

sect.8.6.2 Device Configuration Data (DCD)

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf

for parallel NOR example one can look at sect.4.4.1.4 Flashing U-Boot on Parallel

NOR from U-Boot attached Linux Guide

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
5,988 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Mahesh

for parallel NOR it is placed on 0x1000 bytes offset and described in

sect.8.6.2 Device Configuration Data (DCD)

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf

for parallel NOR example one can look at sect.4.4.1.4 Flashing U-Boot on Parallel

NOR from U-Boot attached Linux Guide

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复