DCD (Device Configuration Data) for i.Mx6 QuadCore

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DCD (Device Configuration Data) for i.Mx6 QuadCore

ソリューションへジャンプ
8,049件の閲覧回数
maheshkumarkoda
Contributor III

Is it possible to modify DCD (Device Configuration Data)? or DCD is hard coded for internal ROM to boot up?

Customized Hardware board with i.Mx6 Quadcore is used in my project.

Also put some light on how DCD is related to pNOR flash with an example?

Thanks a lot :smileyhappy:

ラベル(2)
タグ(3)
0 件の賞賛
返信
1 解決策
7,121件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Mahesh

for parallel NOR it is placed on 0x1000 bytes offset and described in

sect.8.6.2 Device Configuration Data (DCD)

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf

for parallel NOR example one can look at sect.4.4.1.4 Flashing U-Boot on Parallel

NOR from U-Boot attached Linux Guide

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
7,122件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Mahesh

for parallel NOR it is placed on 0x1000 bytes offset and described in

sect.8.6.2 Device Configuration Data (DCD)

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf

for parallel NOR example one can look at sect.4.4.1.4 Flashing U-Boot on Parallel

NOR from U-Boot attached Linux Guide

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信