DART-MX8M-MINI File in wrong format

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DART-MX8M-MINI File in wrong format

1,388 Views
dadi
Contributor I

Hello,

I try to build a yocto image for DART-MX8M-MINI following this instructions but i got this error:

var-fsl-yocto/build_xwayland/tmp/work/aarch64-poky-linux/assimp/4.1.0-r0/recipe-sysroot-native/usr/lib/libz.so: error adding symbols: File in wrong format
| collect2: error: ld returned 1 exit status
| ninja: build stopped: subcommand failed.
| WARNING: exit code 1 from a shell command.
| ERROR: Function failed: do_compile (log file is located at ....../var-fsl-yocto/build_xwayland/tmp/work/aarch64-poky-linux/assimp/4.1.0-r0/temp/log.do_compile.30773)
ERROR: Task (......../var-fsl-yocto/sources/poky/meta/recipes-graphics/vulkan/assimp_4.1.0.bb:do_compile) failed with exit code '1'

 

Any idea how to fix it?

 

 

Labels (1)
0 Kudos
Reply
1 Reply

1,343 Views
Rita_Wang
NXP TechSupport
NXP TechSupport
0 Kudos
Reply