Custom IMX8MM based in EVKD4 won't Boot and no Serial output

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Custom IMX8MM based in EVKD4 won't Boot and no Serial output

1,125件の閲覧回数
Jay_Pineda
Contributor I

Details:

1. Custom Board based on EVK-DDR4

2. Passed the MScale DDR test and Stress

3. Bootloader build s based on the DDR4 Timing Mscale Tool

4. UUU tool successfully downloaded the boot file to imx8 but no response on UART4 debug

5. All power rain of PMIC BD71847 is confirmed correct. 

6. BootMode[1:0] = 01 ( Serial Download)

No Boot response in terminal 

ラベル(1)
0 件の賞賛
返信
1 返信

1,098件の閲覧回数
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @Jay_Pineda,

I hope you are doing well.

Do you see any logs on the UART4 console while flashing the processor in USB Serial Download mode?
If no, have you made all the required changes to change the debug console to UART4 since the default A-core debug console is UART2?

Thanks & Regards,
Ritesh M Patel

0 件の賞賛
返信