Unable to detect Logitech C270 Camera on iMX8 qm on android 11r40

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Unable to detect Logitech C270 Camera on iMX8 qm on android 11r40

1,660 次查看
swayamdhondge10
Contributor II

We are building an android application that uses camera via USB. But we are unable to detect the camera. We have connected the USB camera over the type C port of the imx8 qm board via a type C OTG.The application works successfully on mobile device.
Requesting your help on this issue. 
Please find the logs we get while running the application in the attached file.


#imx8QM #androidautomotive #camera 

0 项奖励
回复
1 回复

1,624 次查看
prakashram72
Contributor III

Hi @swayamdhondge10 

Based on your description, it seems like the issue might be related to the USB configuration or the Android Camera API compatibility with the iMX8 QM board. Here are a few suggestions:

 

1. Check the USB Configuration: Ensure that the USB Type-C port on the iMX8 QM board is configured correctly to handle the camera data. You can refer to the iMX8 QM board documentation on the NXP community for more details on how to configure the USB ports.

2. Check the Android Camera API: The Android application might be using a version of the Camera API that is not fully compatible with the iMX8 QM board. You might need to modify the application to use a version of the API that is compatible with the board. You can refer to the Android documentation on the NXP community for more details on the supported versions of the Camera API.

3. Check the Camera Compatibility: Not all USB cameras are compatible with the iMX8 QM board. You might need to use a different camera that is known to be compatible with the board. You can refer to the iMX8 QM board documentation on the NXP community for a list of compatible cameras.

4. Check the Logs: The logs that you have attached might contain more information about the issue. Look for any error messages or warnings related to the USB connection or the Camera API. These messages might give you a clue about what is causing the issue.

5. Check the Power Supply: The USB Type-C port on the iMX8 QM board might not be able to supply enough power to the camera. You might need to use an external power supply for the camera.

 

Without more specific information about the issue, it's hard to provide a more detailed solution. However, I hope these suggestions will help you troubleshoot the issue. If you need more help, please provide more details about the issue, such as the exact error messages you are seeing in the logs, the version of the Android Camera API you are using, and the model of the USB camera you are trying to use.

Regards,

Prakash

0 项奖励
回复