Custom Data Saving in eFuse

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Custom Data Saving in eFuse

ソリューションへジャンプ
1,619件の閲覧回数
jacky_cheng
Contributor I

Hi Community,

I want to save some custom data into eFuse. After reading the iMX7 - Reference Manual, I think "OCOTP_GP" can be used and will not affect the operation.

However, the size of that register is not enough. Is there have other register can be used to save custom data and will not have any effect?

Thanks,

Jacky

0 件の賞賛
返信
1 解決策
1,554件の閲覧回数
art
NXP Employee
NXP Employee

Q. Is there have other register can be used to save custom data and will not have any effect?

A. No, the OCOTP_GPx fuse words are the only ones that can be used for general purpose software tasks without any side effect.


Have a great day,
Artur

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,555件の閲覧回数
art
NXP Employee
NXP Employee

Q. Is there have other register can be used to save custom data and will not have any effect?

A. No, the OCOTP_GPx fuse words are the only ones that can be used for general purpose software tasks without any side effect.


Have a great day,
Artur

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信