Current sinking capability of iMX7 GPIOs when configured as Open Drain outputs

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Current sinking capability of iMX7 GPIOs when configured as Open Drain outputs

1,426 次查看
DeepakKukreja
Contributor III

Hi,

I was trying to find the current sinking abillity of GPIO pins of the iM7D SoC when configured as open drain output.

I could find the current sinking/sourcing capability for Push/Pull outputs but not for open drain outputs in the iMX7 datasheet:

pastedImage_1.png

A peripheral pin would be driving a CMOS Chip that is biased (supply voltage is at 5V). So I was thinking if it is possible to configure this pin(iMX7) as open drain and pull it up through a resistor to 5V to interface these devices.

标记 (2)
0 项奖励
回复
1 回复

1,182 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Deepak

for open drain such data is not specified and it can be considered the same

as current sinking/sourcing capability for Push/Pull outputs. It is not possible to

pull it up through a resistor to 5V as input voltage should not exceed OVDD+0.3V

according to Table 7. Absolute maximum ratings datasheet. Also there are protection

diodes at pad connected to OVDD and ground.

http://cache.nxp.com/files/32bit/doc/data_sheet/IMX7DCEC.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复