Current Issue : High current value after poweroff

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Current Issue : High current value after poweroff

2,700 Views
snan1z
Contributor I

Hi,

 

I'm dealing with an i.mx28 project whose products will enter standby mode if power is down and in the standby mode it will use battery(3.6V, 400mA). But in the standby mode(after poweroff command), it spents 60mA and it is so high for us.

 

How can i decrease spent current in the standby mode ?

 

Thanks for any help.

 

Best Regards,

Sinan

Labels (1)
0 Kudos
Reply
3 Replies

2,484 Views
chrdcv
Contributor II

Hello!

You can check my post: IMX287 Power Supply Issues

Maybe the answer of your question too.

BR,

Christian

0 Kudos
Reply

2,484 Views
snan1z
Contributor I
Sorry for mistake, it is 400mA/h
0 Kudos
Reply

2,484 Views
chrdcv
Contributor II

Hello snan snan! I'm faced the same trouble! Anyone can help-me?

0 Kudos
Reply