Current Issue : High current value after poweroff

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Current Issue : High current value after poweroff

1,986 次查看
snan1z
Contributor I

Hi,

 

I'm dealing with an i.mx28 project whose products will enter standby mode if power is down and in the standby mode it will use battery(3.6V, 400mA). But in the standby mode(after poweroff command), it spents 60mA and it is so high for us.

 

How can i decrease spent current in the standby mode ?

 

Thanks for any help.

 

Best Regards,

Sinan

标签 (1)
0 项奖励
回复
3 回复数

1,770 次查看
chrdcv
Contributor II

Hello!

You can check my post: IMX287 Power Supply Issues

Maybe the answer of your question too.

BR,

Christian

0 项奖励
回复

1,770 次查看
snan1z
Contributor I
Sorry for mistake, it is 400mA/h
0 项奖励
回复

1,770 次查看
chrdcv
Contributor II

Hello snan snan! I'm faced the same trouble! Anyone can help-me?

0 项奖励
回复