Critical temperature on IMX8M Mini

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Critical temperature on IMX8M Mini

3,050件の閲覧回数
DanielDuJijun
Contributor III

When we did the imx8mm test, we encountered the system warning that the temperature was too high, reaching 95 degrees, I would like to ask why there was a warning at 95 degrees when we were using an industrial grade chip and the theoretical temperature should be able to reach 105 degrees.

0 件の賞賛
返信
4 返答(返信)

3,049件の閲覧回数
DanielDuJijun
Contributor III

DanielDuJijun_0-1716779220910.png

 

0 件の賞賛
返信

3,013件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @DanielDuJijun 

Can you share the kernel version?

0 件の賞賛
返信

3,010件の閲覧回数
DanielDuJijun
Contributor III

Linux Kernel : L5.10.72 

0 件の賞賛
返信

2,989件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @DanielDuJijun 

The temperatures are read from TMU on SOC, you can modify them with thermal sysfs.

echo 105000 > /sys/class/thermal/thermal_zone0/trip_point_1_temp

 

0 件の賞賛
返信