Create SBOM iMX8QM android 12

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Create SBOM iMX8QM android 12

2,346 次查看
sig0912
Contributor III

Hi everyone!

I am trying to build the sbom for my custom board but with no success.

I am following these steps as specified in the Android guide to build the sbom
https://source.android.com/docs/setup/create/create-sbom

$ source build/envsetup.sh
$ lunch mek_8q_car2-userdebug
$ m sbom # Generates an SBOM

It looks like the target 'sbom' is not supported by the Android platform for i.MX as it is not recognized during the build.

Does anyone has any experience with generating sbom?

Thanks in advance

0 项奖励
回复
3 回复数

2,331 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

The application is not supported by default in MX8 but which error are you seeing when you installed?

regards

 

0 项奖励
回复

2,235 次查看
sig0912
Contributor III

Hello,

Can you please explain which application needs to be installed for sbom generation?

Thanks

Best Regards

0 项奖励
回复

2,309 次查看
sig0912
Contributor III

Hi! 

Thanks for the quick response.
After running s bom, I get FAILED: ninja: unknow target 's bom'

Capture.PNG

0 项奖励
回复