Create Android 7.1.2 image on SD for imx6 DL SABRE-AI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Create Android 7.1.2 image on SD for imx6 DL SABRE-AI

3,930 Views
markmao
Contributor I

Hi 

My Imx6 DL Sabre-AI board comes with a empty SD card. So I download Android 7.1.2 image and try to flash to SD card by using mfgtool. But I got the following error: 

UTP: received command '$ simg2img $FILE /dev/mmcblk2p5'
UTP: executing "simg2img $FILE /dev/mmcblk2p5"
Failed to read sparse file
UTP: sending Non-success to kernel for command $ simg2img $FILE /dev/mmcblk2p5.
utp_poll: exit with status 65280
If I use this mfgtool 5.0 (link). I got the error is the boot partition is too small to copy.

Can anybody tell me where can I find the correct MFGTOOL to create SD image

Please see the full log below:

U-Boot 2016.03-imx_v2016.03_4.1.15_2.0.0_ga+g0ec2a01 (Sep 16 2016 - 18:21:34 -0500)

CPU: Freescale i.MX6DL rev1.1 at 792MHz
CPU: Commercial temperature grade (0C to 95C) at 40C
Reset cause: POR
Board: MX6Q-Sabreauto revA
I2C: ready
DRAM: 2 GiB
PMIC: PFUZE100 ID=0x10
NAND: 0 MiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1
*** Warning - bad CRC, using default environment

No panel detected: default to Hannstar-XGA
Display: Hannstar-XGA (1024x768)
In: serial
Out: serial
Err: serial
switch to partitions #0, OK
mmc1 is current device
Net: FEC [PRIME]
Boot from USB for mfgtools
Use default environment for mfgtools
Run bootcmd_mfg: run mfgtool_args;bootz ${loadaddr} ${initrd_addr} ${fdt_addr};
Hit any key to stop autoboot: 0
Kernel image @ 0x12000000 [ 0x000000 - 0x554130 ]
## Loading init Ramdisk from Legacy Image at 12c00000 ...
Image Name: fsl-image-mfgtool-initramfs-imx6
Image Type: ARM Linux RAMDisk Image (gzip compressed)
Data Size: 8591032 Bytes = 8.2 MiB
Load Address: 00000000
Entry Point: 00000000
Verifying Checksum ... OK
## Flattened Device Tree blob at 18000000
Booting using the fdt blob at 0x18000000
Using Device Tree in place at 18000000, end 1800e359

Starting kernel ...

Booting Linux on physical CPU 0x0
Linux version 4.1.15+ (bamboo@yb6) (gcc version 5.3.0 (GCC) ) #1 SMP PREEMPT Fri Sep 16 18:10:49 CDT 2016
CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c5387d
CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine model: Freescale i.MX6 DualLite/Solo SABRE Automotive Board
Reserved memory: created CMA memory pool at 0x6a000000, size 320 MiB
Reserved memory: initialized node linux,cma, compatible id shared-dma-pool
Memory policy: Data cache writealloc
PERCPU: Embedded 12 pages/cpu @ee718000 s16716 r8192 d24244 u49152
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 520720
Kernel command line: console=ttymxc3,115200 rdinit=/linuxrc g_mass_storage.stall=0 g_mass_storage.removable=1 g_mass_storage.file=/fat g_mass_storage.ro=1 g_mass_storage.idVendor=0x066F g_mass_storage.idProduct=0x37FF g_mass_storage.iSerialNumber= enable_wait_mode=off
PID hash table entries: 4096 (order: 2, 16384 bytes)
Dentry cache hash table entries: 262144 (order: 8, 1048576 bytes)
Inode-cache hash table entries: 131072 (order: 7, 524288 bytes)
Memory: 1731696K/2097152K available (6903K kernel code, 320K rwdata, 2416K rodata, 384K init, 423K bss, 37776K reserved, 327680K cma-reserved, 270336K highmem)
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
vmalloc : 0xf0000000 - 0xff000000 ( 240 MB)
lowmem : 0x80000000 - 0xef800000 (1784 MB)
pkmap : 0x7fe00000 - 0x80000000 ( 2 MB)
modules : 0x7f000000 - 0x7fe00000 ( 14 MB)
.text : 0x80008000 - 0x80921fd8 (9320 kB)
.init : 0x80922000 - 0x80982000 ( 384 kB)
.data : 0x80982000 - 0x809d2080 ( 321 kB)
.bss : 0x809d5000 - 0x80a3ee54 ( 424 kB)
SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
Preemptible hierarchical RCU implementation.
Additional per-CPU info printed with stalls.
RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=2.
RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
NR_IRQS:16 nr_irqs:16 16
L2C-310 erratum 769419 enabled
L2C-310 enabling early BRESP for Cortex-A9
L2C-310 full line of zeros enabled for Cortex-A9
L2C-310 ID prefetch enabled, offset 16 lines
L2C-310 dynamic clock gating enabled, standby mode enabled
L2C-310 cache controller enabled, 16 ways, 512 kB
L2C-310: CACHE_ID 0x410000c8, AUX_CTRL 0x76450001
mxc_clocksource_init 3000000
Switching to timer-based delay loop, resolution 333ns
sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 715827882841ns
clocksource mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 637086815595 ns
Console: colour dummy device 80x30
Calibrating delay loop (skipped), value calculated using timer frequency.. 6.00 BogoMIPS (lpj=30000)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 4096 (order: 2, 16384 bytes)
Mountpoint-cache hash table entries: 4096 (order: 2, 16384 bytes)
CPU: Testing write buffer coherency: ok
CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
Setting up static identity map for 0x10008280 - 0x100082f0
CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
Brought up 2 CPUs
SMP: Total of 2 processors activated (12.00 BogoMIPS).
CPU: All CPU(s) started in SVC mode.
devtmpfs: initialized
VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
clocksource jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
pinctrl core: initialized pinctrl subsystem
NET: Registered protocol family 16
DMA: preallocated 256 KiB pool for atomic coherent allocations
cpuidle: using governor ladder
cpuidle: using governor menu
CPU identified as i.MX6DL, silicon rev 1.1
hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
hw-breakpoint: maximum watchpoint size is 4 bytes.
imx6dl-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver
imx-gpc 20dc000.gpc: no fsl,ldo-bypass found!
mxs-dma 110000.dma-apbh: initialized
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
2000000.aips-bus:usbphy_nop1 supply vcc not found, using dummy regulator
2000000.aips-bus:usbphy_nop2 supply vcc not found, using dummy regulator
i2c i2c-1: IMX I2C adapter registered
i2c i2c-1: can't use DMA
i2c i2c-2: IMX I2C adapter registered
i2c i2c-2: can't use DMA
Linux video capture interface: v2.00
pps_core: LinuxPPS API ver. 1 registered
pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
PTP clock support registered
imx-ipuv3 2400000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
Advanced Linux Sound Architecture Driver Initialized.
Switched to clocksource mxc_timer1
NET: Registered protocol family 2
TCP established hash table entries: 16384 (order: 4, 65536 bytes)
TCP bind hash table entries: 16384 (order: 5, 131072 bytes)
TCP: Hash tables configured (established 16384 bind 16384)
UDP hash table entries: 1024 (order: 3, 32768 bytes)
UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
Trying to unpack rootfs image as initramfs...
Freeing initrd memory: 8392K (82c00000 - 83432000)
CPU PMU: Failed to parse /soc/pmu/interrupt-affinity[0]
hw perfevents: enabled with armv7_cortex_a9 PMU driver, 7 counters available
imx rpmsg driver is registered.
Bus freq driver module loaded
futex hash table entries: 512 (order: 3, 32768 bytes)
VFS: Disk quotas dquot_6.6.0
VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
NFS: Registering the id_resolver key type
Key type id_resolver registered
Key type id_legacy registered
jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
fuse init (API version 7.23)
bounce: pool size: 64 pages
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
backlight supply power not found, using dummy regulator
mxc_sdc_fb fb@0: NO mxc display driver found!
mxc_sdc_fb fb@1: NO mxc display driver found!
imx-sdma 20ec000.sdma: no iram assigned, using external mem
imx-sdma 20ec000.sdma: no event needs to be remapped
imx-sdma 20ec000.sdma: loaded firmware 3.3
imx-sdma 20ec000.sdma: initialized
pfuze100-regulator 1-0008: Full layer: 1, Metal layer: 1
pfuze100-regulator 1-0008: FAB: 0, FIN: 0
pfuze100-regulator 1-0008: pfuze100 found.
21ec000.serial: ttymxc2 at MMIO 0x21ec000 (irq = 299, base_baud = 5000000) is a IMX
21f0000.serial: ttymxc3 at MMIO 0x21f0000 (irq = 300, base_baud = 5000000) is a IMX
console [ttymxc3] enabled
imx sema4 driver is registered.
[drm] Initialized drm 1.1.0 20060810
[drm] Initialized vivante 1.0.0 20120216 on minor 0
brd: module loaded
loop: module loaded
2188000.ethernet supply phy not found, using dummy regulator
pps pps0: new PPS source ptp0
libphy: fec_enet_mii_bus: probed
fec 2188000.ethernet eth0: registered PHC device 0
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
ehci-mxc: Freescale On-Chip EHCI Host driver
usbcore: registered new interface driver usb-storage
2184800.usbmisc supply vbus-wakeup not found, using dummy regulator
imx_usb 2184000.usb: Can't register ci_hdrc platform device, err=-517
imx_usb 2184200.usb: Can't register ci_hdrc platform device, err=-517
udc-core: couldn't find an available UDC - added [g_mass_storage] to list of pending drivers
mousedev: PS/2 mouse device common for all mice
egalax_ts 1-0004: Failed to read firmware version
egalax_ts: probe of 1-0004 failed with error -5
snvs_rtc 20cc000.snvs:snvs-rtc-lp: rtc core: registered 20cc000.snvs:snvs-r as rtc0
i2c /dev entries driver
IR NEC protocol handler initialized
IR RC5(x/sz) protocol handler initialized
IR RC6 protocol handler initialized
IR JVC protocol handler initialized
IR Sony protocol handler initialized
IR SANYO protocol handler initialized
IR Sharp protocol handler initialized
IR MCE Keyboard/mouse protocol handler initialized
IR XMP protocol handler initialized
imx2-wdt 20bc000.wdog: timeout 60 sec (nowayout=0)
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
/soc/aips-bus@02100000/usdhc@02190000: voltage-ranges unspecified
sdhci-esdhc-imx 2190000.usdhc: Got CD GPIO
sdhci-esdhc-imx 2190000.usdhc: No vmmc regulator found
sdhci-esdhc-imx 2190000.usdhc: No vqmmc regulator found
mmc0: SDHCI controller on 2190000.usdhc [2190000.usdhc] using ADMA
/soc/aips-bus@02100000/usdhc@02198000: voltage-ranges unspecified
sdhci-esdhc-imx 2198000.usdhc: Got CD GPIO
sdhci-esdhc-imx 2198000.usdhc: Got WP GPIO
sdhci-esdhc-imx 2198000.usdhc: No vmmc regulator found
sdhci-esdhc-imx 2198000.usdhc: No vqmmc regulator found
mmc2: SDHCI controller on 2198000.usdhc [2198000.usdhc] using ADMA
218c000.mlb supply reg_nvcc not found, using dummy regulator
mxc_mlb150 218c000.mlb: enalbe regulator
mxc_vpu 2040000.vpu_fsl: VPU initialized
mxc_vdoa 21e4000.vdoa: i.MX Video Data Order Adapter(VDOA) driver probed
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
mmc2: new high speed SDHC card at address aaaa
mmcblk2: mmc2:aaaa SU08G 7.40 GiB
mmcblk2: p1 p2 p3 < p5 p6 p7 p8 p9 p10 p11 p12 > p4
imx-spdif sound-spdif: snd-soc-dummy-dai <-> 2004000.spdif mapping ok
NET: Registered protocol family 10
sit: IPv6 over IPv4 tunneling driver
NET: Registered protocol family 17
Key type dns_resolver registered
Registering SWP/SWPB emulation handler
Mass Storage Function, version: 2009/09/11
LUN: removable file: (no medium)
LUN: removable read only file: /fat
Number of LUNs=1
Number of LUNs=1
g_mass_storage gadget: Mass Storage Gadget, version: 2009/09/11
g_mass_storage gadget: g_mass_storage ready
ci_hdrc ci_hdrc.1: EHCI Host Controller
ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1
ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
input: gpio-keys as /devices/soc0/gpio-keys/input/input1
snvs_rtc 20cc000.snvs:snvs-rtc-lp: setting system clock to 1970-01-01 00:00:00 UTC (0)
can-stby: disabling
can-en: disabling
usb_otg_vbus: disabling
VGEN2: disabling
SW4: disabling
ALSA device list:
#0: imx-spdif
Freeing unused kernel memory: 384K (80922000 - 80982000)
Starting UTP
uuc 0.5 [built Sep 16 2016 02:36:28]
UTP: Waiting for device to appear
UTP: file/device node /dev/utp already exists
cpu_id is 0
g_mass_storage gadget: high-speed config #1: Linux File-Backed Storage
UTP: received command 'send'
UTP: sending Success to kernel for command send.
UTP: received command '$ tar xf $FILE '
UTP: executing "tar xf $FILE "
UTP: sending Success to kernel for command $ tar xf $FILE .
utp_poll: pass returned.
UTP: received command '$ sh mksdcard-android.sh /dev/mmcblk2'
UTP: executing "sh mksdcard-android.sh /dev/mmcblk2"
1+0 records in
1+0 records out
1024 bytes (1.0 kB, 1.0 KiB) copied, 0.0246427 s, 41.6 kB/s
Checking that no-one is using thirandom: sfdisk urandom read with 14 bits of entropy available
s disk right now ... OK

Disk /dev/mmcblk2: 7.4 GiB, 7948206080 bytes, 15523840 sectors
Units: sectors of 1 * 512 = 512 bytes
Sector size (logical/physical): 512 bytes / 512 bytes
I/O size (minimum/optimal): 512 bytes / 512 bytes

>>> Created a new DOS disklabel with disk identifier 0x5c092038.
Created a new partition 1 of type 'Linux' and of size 24 MiB.
/dev/mmcblk2p2: Created a new partition 2 of type 'Linux' and of size 16 M mmcblk2: p1 p2 p3 < p5 p6 p7 p8 p9 p10 p11 p12 > p4
iB.
/dev/mmcblk2p3: Created a new partition 3 of type 'Extended' and of size 1.3 GiB.
/dev/mmcblk2p4: Created a new partition 4 of type 'Linux' and of size 6 GiB.
/dev/mmcblk2p5: Created a new partition 5 of type 'Linux' and of size 800 MiB.
/dev/mmcblk2p6: Created a new partition 6 of type 'Linux' and of size 512 M mmcblk2: p1 p2 p3 < p5 p6 p7 p8 p9 p10 p11 p12 > p4
iB.
/dev/mmcblk2p7: Created a new partition 7 of type 'Linux' and of size 8 MiB.
/dev/mmcblk2p8: Created a new partition 8 of type 'Linux' and of size 4 MiB.
/dev/mmcblk2p9: Created a new partition 9 of type 'Linux' and of size 2 MiB.
/dev/mmcblk2p10: C mmcblk2: p1 p2 p3 < p5 p6 p7 p8 p9 p10 p11 p12 > p4
reated a new partition 10 of type 'Linux' and of size 2 MiB.
/dev/mmcblk2p11: Created a new partition 11 of type 'Linux' and of size 1 MiB.
/dev/mmcblk2p12: Created a new partition 12 of type 'Linux' and of size 1 MiB.
/dev/mmcblk2p13:
New situation:

Device Boot Start End Sectors Size Id Type
/dev/mmcblk2p1 2048 51199 49152 24M 83 Linux
/dev/mmcblk2p2 51200 83967 32768 16M 83 Linux
/dev/mmcblk2p3 83968 2889727 2805760 1.3G 5 Extended
/dev/mmcblk2p4 2889728 15523839 12634112 6G 83 Linux
/dev/mmcblk2p5 86016 1724415 1638400 800M 83 Linux
/dev/mmcblk2p6 1726464 2775039 1048576 512M 83 Linux
/dev/mmcblk2p7 2777088 2793471 16384 8M 83 Linux
/dev/mmcblk2p8 2795520 2803711 8192 4M 83 Linux
/dev/mmcblk2p9 2805760 2809855 4096 2M 83 Linux
/dev/mmcblk2p10 2811904 2815999 4096 2M 83 Linux
/dev/mmcblk2p11 2818048 2820095 2048 1M 83 Linux
/dev/mmcblk2p12 2822144 2824191 2048 1M 83 Linux

Partition table entries are not in disk order.

The partition table has been altered.
Calling ioctl() to re-read partition table.
Syncing disks.
Checking that no-one is using this disk right now ... OK

Disk /dev/mmcblk2: 7.4 GiB, 7948206080 bytes, 15523840 sectors
Units: sectors of 1 * 512 = 512 bytes
Sector size (logical/physical): 512 bytes / 512 bytes
I/O size (minimum/optimal): 512 bytes / 512 bytes
Disklabel type: dos
Disk identifier: 0x5c092038

Old situation:

Device Boot Start End Sectors Size Id Type
/dev/mmcblk2p1 2048 51199 49152 24M 83 Linux
/dev/mmcblk2p2 51200 83967 32768 16M 83 Linux
/dev/mmcblk2p3 83968 2889727 2805760 1.3G 5 Extended
/dev/mmcblk2p4 2889728 15523839 12634112 6G 83 Linux
/dev/mmcblk2p5 86016 1724415 1638400 800M 83 Linux
/dev/mmcblk2p6 1726464 2775039 1048576 512M 83 Linux
/dev/mmcblk2p7 2777088 2793471 16384 8M 83 Linux
/dev/mmcblk2p8 2795520 2803711 8192 4M 83 Linux
/dev/mmcblk2p9 2805760 2809855 4096 2M 83 Linux
/dev/mmcblk2p10 2811904 2815999 4096 2M 83 Linux
/dev/mmcblk2p11 2818048 2820095 2048 1M 83 Linux
/dev/mmcblk2p12 2822144 2824191 2048 1M 83 Linux

Partition table entries are not in disk order.

/dev/mmcblk2p1:
New situation:

Device Boot Start End Sectors Size Id Type
/dev/mmcblk2p1 16384 49151 32768 16M 83 Linux
/dev/mmcblk2p2 51200 83967 32768 16M 83 Linux
/dev/mmcblk2p3 83968 2889727 2805760 1.3G 5 Extended
/dev/mmcblk2p4 2889728 15523839 12634112 6G 83 Linux
/dev/mmcblk2p5 86016 1724415 1638400 800M 83 Linux
/dev/mmcblk2p6 1726464 2775039 1048576 512M 83 Linux
/dev/mmcblk2p7 2777088 2793471 16384 8M 83 Linux
/dev/mmcblk2p8 2795520 2803711 8192 4M 83 Linux
/dev/mmcblk2p9 2805760 2809855 4096 2M 83 Linux
/dev/mmcblk2p10 2811904 2815999 4096 2M 83 Linux
/dev/mmcblk2p11 2818048 2820095 2048 1M 83 Linux
/dev/mmcblk2p12 2822144 2824191 2048 1M 83 Linux

Partition table entries are not in disk order.

The partition table has been altered.
Calling ioctl() to re-read partition table.
Syncing disks.
formating android data partition
mke2fs 1.43-WIP (18-May-2015)
Creating filesystem with 1579264 4k blocks and 395136 inodes
Filesystem UUID: cb80c3df-7d07-4157-9ab7-79ae82e2e38a
Superblock backups stored on blocks:
32768, 98304, 163840, 229376, 294912, 819200, 884736

Allocating group tables: done
Writing inode tables: done
Creating journal (32768 blocks): done
Writing superblocks and filesystem accounting information: random: nonblocking pool is initialized
done

UTP: sending Success to kernel for command $ sh mksdcard-android.sh /dev/mmcblk2.
utp_poll: pass returned.
UTP: received command 'send'
UTP: sending Success to kernel for command send.
UTP: received command '$ dd if=/dev/zero of=/dev/mmcblk2 bs=1k seek=768 conv=fsync count=8'
UTP: executing "dd if=/dev/zero of=/dev/mmcblk2 bs=1k seek=768 conv=fsync count=8"
8+0 records in
8+0 records out
8192 bytes (8.2 kB, 8.0 KiB) copied, 0.0131797 s, 622 kB/s
UTP: sending Success to kernel for command $ dd if=/dev/zero of=/dev/mmcblk2 bs=1k seek=768 conv=fsync count=8.
utp_poll: pass returned.
UTP: received command '$ dd if=$FILE of=/dev/mmcblk2 bs=1k seek=1 conv=fsync'
UTP: executing "dd if=$FILE of=/dev/mmcblk2 bs=1k seek=1 conv=fsync"
591+0 records in
591+0 records out
605184 bytes (605 kB, 591 KiB) copied, 0.278617 s, 2.2 MB/s
UTP: sending Success to kernel for command $ dd if=$FILE of=/dev/mmcblk2 bs=1k seek=1 conv=fsync.
utp_poll: pass returned.
UTP: received command '$ ls -l /dev/mmc* '
UTP: executing "ls -l /dev/mmc* "
brw------- 1 root root 179, 0 Jan 1 00:01 /dev/mmcblk2
brw------- 1 root root 179, 1 Jan 1 00:00 /dev/mmcblk2p1
brw------- 1 root root 179, 10 Jan 1 00:00 /dev/mmcblk2p10
brw------- 1 root root 179, 11 Jan 1 00:00 /dev/mmcblk2p11
brw------- 1 root root 179, 12 Jan 1 00:00 /dev/mmcblk2p12
brw------- 1 root root 179, 2 Jan 1 00:00 /dev/mmcblk2p2
brw------- 1 root root 179, 3 Jan 1 00:00 /dev/mmcblk2p3
brw------- 1 root root 179, 4 Jan 1 00:01 /dev/mmcblk2p4
brw------- 1 root root 179, 5 Jan 1 00:00 /dev/mmcblk2p5
brw------- 1 root root 179, 6 Jan 1 00:00 /dev/mmcblk2p6
brw------- 1 root root 179, 7 Jan 1 00:00 /dev/mmcblk2p7
brw------- 1 root root 179, 8 Jan 1 00:00 /dev/mmcblk2p8
brw------- 1 root root 179, 9 Jan 1 00:00 /dev/mmcblk2p9
UTP: sending Success to kernel for command $ ls -l /dev/mmc* .
utp_poll: pass returned.
UTP: received command 'send'
UTP: sending Success to kernel for command send.
UTP: received command '$ dd if=$FILE of=/dev/mmcblk2p1'
UTP: executing "dd if=$FILE of=/dev/mmcblk2p1"
22394+1 records in
22394+1 records out
11466024 bytes (11 MB, 11 MiB) copied, 8.63799 s, 1.3 MB/s
UTP: sending Success to kernel for command $ dd if=$FILE of=/dev/mmcblk2p1.
utp_poll: pass returned.
UTP: received command '$ mkfs.ext4 -F /dev/mmcblk2p5'
UTP: executing "mkfs.ext4 -F /dev/mmcblk2p5"
mke2fs 1.43-WIP (18-May-2015)
Discarding device blocks: done
Creating filesystem with 204800 4k blocks and 51296 inodes
Filesystem UUID: 029ca65f-8a6d-43c4-bb2b-1d658d495250
Superblock backups stored on blocks:
32768, 98304, 163840

Allocating group tables: done
Writing inode tables: done
Creating journal (4096 blocks): done
Writing superblocks and filesystem accounting information: done

UTP: sending Success to kernel for command $ mkfs.ext4 -F /dev/mmcblk2p5.
utp_poll: pass returned.
UTP: received command '$ mkfs.ext4 -F /dev/mmcblk2p6'
UTP: executing "mkfs.ext4 -F /dev/mmcblk2p6"
mke2fs 1.43-WIP (18-May-2015)
Discarding device blocks: done
Creating filesystem with 131072 4k blocks and 32768 inodes
Filesystem UUID: 06d27a95-845c-424f-9df3-7257f30c58d9
Superblock backups stored on blocks:
32768, 98304

Allocating group tables: done
Writing inode tables: done
Creating journal (4096 blocks): done
Writing superblocks and filesystem accounting information: done

UTP: sending Success to kernel for command $ mkfs.ext4 -F /dev/mmcblk2p6.
utp_poll: pass returned.
UTP: received command '$ mkfs.ext4 -F /dev/mmcblk2p7'
UTP: executing "mkfs.ext4 -F /dev/mmcblk2p7"
mke2fs 1.43-WIP (18-May-2015)
Discarding device blocks: done
Creating filesystem with 8192 1k blocks and 2048 inodes

Allocating group tables: done
Writing inode tables: done
Creating journal (1024 blocks): done
Writing superblocks and filesystem accounting information: done

UTP: sending Success to kernel for command $ mkfs.ext4 -F /dev/mmcblk2p7.
utp_poll: pass returned.
UTP: received command '$ mount -o remount,size=600M rootfs /'
UTP: executing "mount -o remount,size=600M rootfs /"
UTP: sending Success to kernel for command $ mount -o remount,size=600M rootfs /.
utp_poll: pass returned.
UTP: received command 'send'
UTP: sending Success to kernel for command send.
UTP: received command '$ simg2img $FILE /dev/mmcblk2p5'
UTP: executing "simg2img $FILE /dev/mmcblk2p5"
Failed to read sparse file
UTP: sending Non-success to kernel for command $ simg2img $FILE /dev/mmcblk2p5.
utp_poll: exit with status 65280

Thanks

Mark

Labels (2)
Tags (1)
0 Kudos
Reply
2 Replies

2,689 Views
markmao
Contributor I

After searching community.nxp I found the MfgTools for Android 7.1.2. So I run this tool and select this setting:

mfgtool2-android-mx6dl-sabreauto-sdcard.vbs

The whole process is passed. But after changing boot mode setting to normal, the board is booting and UART has output. But HDMI has no signal.

Please see the attached log.

Thanks

Android N7.1.2_2.0.0 GA Release Announcement

0 Kudos
Reply

2,689 Views
igorpadykov
NXP Employee
NXP Employee

Hi Mark

for hdmi one can set appropriatekernel boot parameter "video" as described in

Table 25. Kernel boot parameters attached User Guide. Please also check other documents on

https://www.nxp.com/webapp/Download?colCode=IMX_N7.1.2_2.0.0_ANDROID_DOCS 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply