Crash in gcoHAL_QueryChipCount when initializing OpenGLES on i.MX6D

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Crash in gcoHAL_QueryChipCount when initializing OpenGLES on i.MX6D

2,335件の閲覧回数
huib-janimbens
Contributor II

On a MarSBoard with i.MX6 dual ( http://www.embest-tech.com/shop/star/marsboard.html ) I installed a yocto image build using recipes from silmerusse/meta-robomind

After installing I copiedIndex of /buildsources/g/gpu-viv-bin-mx6q/gpu-viv-bin-mx6q-1.1.0 over /usr.

A simple OpenGLES 2.0 app built with -DEGL_API_FB=1 crashes in gcoHAL_QueryChipCount.

A stacktrace:

#0  0x2ab19984 in gcoHAL_QueryChipCount () from /usr/lib/libGAL.so

#1  0x2aaf8ad0 in veglGetThreadData () from /usr/lib/libEGL.so

#2  0x2aaf1f30 in eglGetDisplay () from /usr/lib/libEGL.so

#3  0x00068634 in OpenGLApplication::InitOpenGL (this=0x7efff950) at application.cpp:859

#4  0x00017d70 in main (argc=1, argv=0x7efffd04) at consoleapp.cpp:368

Site of crash:

(gdb) x/8i $pc-16

   0x2ab19974 <gcoHAL_QueryChipCount+28>:       str     r2, [r4]

   0x2ab19978 <gcoHAL_QueryChipCount+32>:

    ldr r2, [pc, #8388608]      ; 0x2ab199d0 <gcoHAL_QueryChipCount+120>

   0x2ab1997c <gcoHAL_QueryChipCount+36>:       ldr     r3, [r3, r2]

   0x2ab19980 <gcoHAL_QueryChipCount+40>:       ldr     r3, [r3, #2809676]

=> 0x2ab19984 <gcoHAL_QueryChipCount+44>:       ldr     r3, [r3, #2809676]

   0x2ab19988 <gcoHAL_QueryChipCount+48>:       sub     r2, r3, #1

   0x2ab1998c <gcoHAL_QueryChipCount+52>:       cmp     r2, #2

   0x2ab19990 <gcoHAL_QueryChipCount+56>:

    bhi 0x2ab199ac <gcoHAL_QueryChipCount+84>

I tried to use gpu-viv-bin-mx6q-3.0.35-4.0.0 (using the softfp files) instead of gpu-viv-bin-mx6q-1.1.0 with similar results.

My questions are:

How does one determine the gpu-viv-bin-mx6q version to use?

How do I fix this crash?

ラベル(5)
0 件の賞賛
返信
2 返答(返信)

1,826件の閲覧回数
huib-janimbens
Contributor II

The crash was caused by using the wrong version of libEGL/GAL. The version I needed was gpu-viv-bin-mx6q-3.0.35-4.1.0.

0 件の賞賛
返信

1,826件の閲覧回数
EinarMar
Contributor IV

Hi

I just wanted to let you know that I was facing similar problems but with the hard-float binaries so I got the gpu-viv-bin-mx6q-3.0.35-4.0.0 and then it stopped crashing.

regards

Einar

0 件の賞賛
返信