Could i.MX6 DL output 32Khz clock signal?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Could i.MX6 DL output 32Khz clock signal?

跳至解决方案
1,857 次查看
高丽哲
Contributor I

The i.MX6 DL has external 32khz crystal, and could i.MX6 DL output a 32khz clock signal, use XTALOSC_REF_CLK_32K ?

Thanks

0 项奖励
回复
1 解答
1,565 次查看
Yuri
NXP Employee
NXP Employee

  The REF_CLK_24M and REF_CLK_32K pins are output signals

to reflect corresponding XTAL ones. Please look at Table 71-1

(XTALOSC External Signals) of the Reference Manual.

  Also, please take a look at the next thread :

"Are i.MX6 REF_CLK_24M REF_CLK_32K bypassed clock from external x'tals?"

  https://community.freescale.com/thread/320656

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,566 次查看
Yuri
NXP Employee
NXP Employee

  The REF_CLK_24M and REF_CLK_32K pins are output signals

to reflect corresponding XTAL ones. Please look at Table 71-1

(XTALOSC External Signals) of the Reference Manual.

  Also, please take a look at the next thread :

"Are i.MX6 REF_CLK_24M REF_CLK_32K bypassed clock from external x'tals?"

  https://community.freescale.com/thread/320656

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,565 次查看
高丽哲
Contributor I

Ok,thanks for your reply!

0 项奖励
回复