Could i.MX6 DL output 32Khz clock signal?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Could i.MX6 DL output 32Khz clock signal?

ソリューションへジャンプ
1,928件の閲覧回数
高丽哲
Contributor I

The i.MX6 DL has external 32khz crystal, and could i.MX6 DL output a 32khz clock signal, use XTALOSC_REF_CLK_32K ?

Thanks

0 件の賞賛
返信
1 解決策
1,636件の閲覧回数
Yuri
NXP Employee
NXP Employee

  The REF_CLK_24M and REF_CLK_32K pins are output signals

to reflect corresponding XTAL ones. Please look at Table 71-1

(XTALOSC External Signals) of the Reference Manual.

  Also, please take a look at the next thread :

"Are i.MX6 REF_CLK_24M REF_CLK_32K bypassed clock from external x'tals?"

  https://community.freescale.com/thread/320656

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,637件の閲覧回数
Yuri
NXP Employee
NXP Employee

  The REF_CLK_24M and REF_CLK_32K pins are output signals

to reflect corresponding XTAL ones. Please look at Table 71-1

(XTALOSC External Signals) of the Reference Manual.

  Also, please take a look at the next thread :

"Are i.MX6 REF_CLK_24M REF_CLK_32K bypassed clock from external x'tals?"

  https://community.freescale.com/thread/320656

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,636件の閲覧回数
高丽哲
Contributor I

Ok,thanks for your reply!

0 件の賞賛
返信