Could IMX6SL boot from NAND?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Could IMX6SL boot from NAND?

ソリューションへジャンプ
1,836件の閲覧回数
shaohang_cui
Contributor I

I didn't see NAND flash in IMX6SLRM Chapter 8 like IMX6ULRM; Also I didn't find pin mux for NAND in imx6sl-pinfunc.h. Does it mean IMX6SL can't boot from NAND?

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 解決策
1,797件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Shaohang

you are right, i.IMX6SL can't boot from NAND.

There is no GPMI(NAND) module in i.MX6SL.


Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
1,798件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Shaohang

you are right, i.IMX6SL can't boot from NAND.

There is no GPMI(NAND) module in i.MX6SL.


Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------